Setting Up Employee Deductions and Earnings
To create and define the codes for each deduction
that may be used in your system, use the Deduction
and Earning Codes form.
Then, to set up each employee's deductions as specified
below, use the Employees
form.
Temporary Deductions (Union, Loans, Garnishes)
To set up temporary deductions for an employee:
- On the Deductions tab, enter the employer's retirement contribution
and specify whether the value is a percentage or an amount.
- If applicable, enter a union deduction:
- In the Union Deduction field, enter the amount of the
deduction, whether a currency amount or a percentate.
- In the Per field, select the type of deduction rate
(whether the amount is to be deducted per hour, as a percent,
or as a fixed, flat rate).
- In the Union Freq field, select the frequency at which
the deduction is to be made.
- In the Union Liab Acct field, enter a valid General
Ledger (G/L) account number to identify the union liability account
that the union deduction is posted against.
- If applicable, to automatically deduct an amount from an employee's
paycheck for a loan, enter:
- In the Loan Deduction field, the amount to be deducted
per deduction, in the domestic currency
- In the Loan Freq field, the frequency at which repayments
should be deducted from the employee's pay
- In the Loan Balance Due field, the amount of the loan
to be repaid
The system stops the deductions when the Loan Balance Due
amount reaches 0 (zero).
- If applicable, to automatically garnish wages from an employee's
paycheck, enter:
Other Deductions and Earnings
On the D & E tab (Employees form),
specify the following for each deduction or earning type:
In the Code field, the deduction or earning type code
When you select a code, the system automatically displays the description
for the deduction or earning in the Description field.
In the Amount field, the amount to be deducted or added
In the Type field, whether it is a percentage of the
employee's pay or a flat domestic currency amount
In the Frequency field, the frequency at which the amount
is to be deducted or added
In the Balance field, the total amount to be deducted
or added
NOTE: If this
field is blank, the amount is deducted or added on an ongoing basis.
Additional Local Taxes
Additional local taxes can be deducted from employee
checks and reported in box 20 of the W-2 form. This deduction method should
only be used when two or more local taxes are necessary.
To set up this deduction, on the Deduction
and Earning Codes form, in the Type field, select either Before
tax deduction from gross pay or Deduction from net pay after tax.
For more information, see the field level Help for that field.
NOTES:
- When a deduction or earning is based on a percentage calculation
and the deduction type on this form is Before tax deduction
from gross pay, the system calculates the amount based on
the employee's gross pay.
- W-2 box 20 works differently with the deduction type Deduction
from net pay after tax than it does with any other type of
deduction. If you use the Deduction from net pay after tax
option with W-2 box 20, the system uses the same base pay used
to calculate the primary city tax when the deduction is based
on a percentage.
CAUTION: Each
additional local tax deduction generates an additional W-2 for each employee
who takes that deduction.
Related Topics
Entering Information
About a New Employee
Making Periodic
Deductions
Setting
Up an Employee for Direct Deposit
Steps for Setting
Up Employees