Get ATP/CTP
	
	This button applies only to APS.
	Click this button to generate a projected availability date for 
	 this transaction. The APS system calculates this date by incrementally 
	 planning the transaction in a temporary copy of the planner database 
	 based on the transaction's input 
	 date.
	This button is available only if these conditions are true:
	
		- The order's Status 
		 must be Ordered or Planned. If the order's status 
		 is Ordered and all the 
		 CO lines are filled, the button is disabled. The Customer 
		 Order Line must also be Planned 
		 or Ordered for the button 
		 to be enabled.
- If this is an estimate line item, the estimate's Status 
		 must be Planned, Working, or Quoted.
- If this is a transfer order line item, the To 
		 Ref Type must be Inventory.
When the planning mode is Infinite 
	 APS, this button appears as Get 
	 ATP. When the planning mode is APS, 
	 the button appears as Get CTP. 
	 The difference between the two modes is this:
	
		- ATP: The date projected 
		 by the "available to promise" calculation considers 
		 the capacity of your resources to be infinite while they are working 
		 on-shift. That is, the possibility that the resources are working 
		 on other demands is not factored into the calculated projected 
		 date for this demand.
- CTP: The "capable 
		 to promise" calculation projects the date by which your resources 
		 can actually complete the order, considering their availability.
The Availability Results dialog 
	 displays the projected date.
	
		NOTES:
		
			- If you are entering a forecast for an MPS item, do not click the Get 
			 ATP/CTP button on the Forecast 
			 form. MPS item forecasts must be planned in the MPS 
			 Processor.
- If the demand is associated with a warehouse in which the 
			 Dedicated Inventory field 
			 is selected, you cannot perform the Get ATP/CTP process. The 
			 error message "Availability cannot be checked for demands 
			 from warehouses with dedicated inventory" displays.
 
	For more information, see "About 
	 Incremental Planning and ATP/CTP."