Select a rule to indicate the conditions under which a forming batch load should be released during an override check. This field is enabled only when Override Review is selected.
| Rule | Description |
|---|---|
| Waiting Time Exceeds Threshold | Release the batch if the time to create the batch is longer than the value specified in the Threshold field, in hours. |
| Dynamic Slack Less Than Threshold | Release the batch if the dynamic slack is smaller than or equal to the value specified in the Threshold field. (Dynamic slack = remaining time to due date minus remaining processing time.) |
| User-Defined Override Rule | Release the batch according to a user-defined rule. For more information, see Writing Custom Batch Override Rules. |