NOTE: See Writing a Custom Scheduler Rule for a summary of the steps required to create custom rules. For more details about the functions described in this topic, see the Simulation Tailoring Support Function Reference (available for download from the Support web site, on the documentation page for the Infor APS Virtual Planning/Simulation product).
The Scheduler uses batch override rules to determine if forming batches should be released even though they have not reached the minimum release quantity.
Before you create custom batch override rules and write the corresponding batch override functions, you should understand the logic used by the override function. This rule is invoked under two conditions:
When the batch override function is called, it determines whether the forming batch should be released.
Your custom override function can have any name that is not a standard user-callable function name.
#include "factor.h" int borl(formbat, batch) FORMBAT *formbat; /* pointer to the forming batch */ BATCHDEF *batch; /* pointer to the batch definition */
The override function accepts two arguments, a pointer to forming batch (Type: FORMBAT *) and a pointer to the batch (Type: BATCHDEF *).
The function returns TRUE (non-zero) if the forming batch should be released or FALSE (zero) if the forming batch should not be released (Type:int).
Here is an example of a batch override function based on the time greater than or equal to the override threshold:
int borl (FORMBAT *formbat, BATCHDEF *batch)
/*-----------------------------------------------------------------
Batch override rule which determines that the forming batch should
be released if it has been waiting longer or equal to the override
threshold.
ARGS:
formbat - pointer to the arriving forming batch
batch - pointer to the batch that this load will follow
RETURNS: true, if it has been waiting too long
false, otherwise
-----------------------------------------------------------------*/
{
double x;
x = cstnow - formbat->fbsttim;
/* If the time the batch has been forming is at least the
threshold, then release the batch */
if (x >= batch->btovth)
{
return(1)
}
else
{
return(0)
}
{
To make your custom override function available to the Scheduler, you must "install" it from ucini1 by calling the function sedfok. This function has two arguments in the following order:
For example, to install the above example rule "borl" in rule position 39:
sedfok (39, borl);