The Projected date is the date the planning or scheduling functions estimate a job, customer order, or other demand can be completed, based on other demands and your current capacity. It can be generated for various types of demands by the Scheduler or the APS system.
| For this demand... | This program generates the Projected date |
|---|---|
| Job order | Scheduler (if job has been scheduled; otherwise APS) |
| Estimate job order | Scheduler |
| Production schedule item | Scheduler (if the PS item has been scheduled; otherwise APS) |
| Customer order, order line, or blanket release | APS (if the CO line is cross-referenced to a job, the job's Projected date will display) |
| MPS order | APS |
| Forecast | APS |
| Project resource or estimate project resource | APS |
| Transfer order line | APS |
The Scheduler may calculate the Projected date of a job order or estimate job order.
The planning functions calculate the Projected date differently depending on whether the item has a routing and whether you are using APS:
The system attempts to plan the order or line item as close to the original input date (such as the Due Date for a customer order line) as possible. Therefore, the displayed Projected date may change based on the date you enter before selecting the Get ATP/CTP button. If the Projected date is calculated to fall outside the defined plan horizon, the message, "[Get CTP] was not successful. The order cannot be made in the current horizon" displays and the Projected date field remains unchanged.
This date also may change every time you run APS Planning. For example, if another order is canceled, some capacity may be available that changes the Projected date for this order or item. Or, if the resource that produces an item is off-shift or allocated to a higher-priority order, the Projected date for the item changes.
NOTE: The Projected Date is the date that the APS Planning engine has determined the resource will be available for use on the project. The Late Alert indicator logic compares the Due Date to the Projected Date to determine whether the resource is late or projected to be late.
The Projected field on the Planning Detail form displays different dates depending on the type of demand/supply record that is displayed:
| For this Demand/Supply Record... | the Projected field contains |
|---|---|
| Forecast | Projected date |
| Customer order line item | Projected date |
| Transfer order line item (demand) | Projected date |
| Transfer order line item (supply) | Projected date |
| Project material | Start date (of the project task) |
| Job supply | Projected date |
| PO item | Due date |
| PO Requisition item | Due date |