This field applies to APS.
Enter the maximum number of resource combinations the system will check while trying to pull plan a single operation. This parameter works like the Push Iterations parameter, except during pull-planning passes. We recommend you leave this parameter set to 0 to allow the system to find the fastest resource combination.
For example, an operation specifies 2 resource groups, each with 25 member resources. If the Pull Iteration is set to 10, the system considers only the first 10 combinations of resources when trying to pull plan the operation. If it doesn't find a combination that leaves enough time to finish the remaining operations in the routing, the pull-planning pass fails and the system push plans the operation.