Pull planning is the process APS uses to backward plan a demand from its need date. Starting with the last operation in the end item's routing, the system searches for available supplies (such as purchase orders), inventory, and/or resources to complete the demand on time. The pull-planning process follows this sequence:
NOTE: These steps do not reflect every decision and assumption APS makes. These steps are intended to convey the general pull-planning process.
For any unsatisfied demand quantity, search backward from the due date to allocate on-hand inventory. If sufficient inventory is on hand to satisfy the demand, the planning is complete.
NOTE: When APS allocates inventory to a demand, it considers the combined total of all inventory at all warehouses (at a given site) in which the Dedicated Inventory option is NOT selected.
For any unsatisfied demand quantity, create a planned order. The type of item determines how the system creates the planned order:
| Does item have a routing? | Infinite APS Behavior | APS Behavior |
|---|---|---|
| Yes | Infinite APS pull plans the operations through the
item's routing, starting with the end item's last operation.
It determines the operation start dates by summing the
Move, Queue, Setup, Run, and Finish times defined for
the operations and assumes infinite
resource capacity.
After pull-planning the item through its routing, Infinite APS pull-plans the item's components. The setting of the Plan Materials at Operation Start field determines how the system sets the need date of a component requirement; if the parameter is selected, the need date of a component is the start date of the operation in which it is needed. If the parameter is cleared, the need date is the start date of the job. |
APS plans the operations in the same manner as Infinite
APS in almost all respects.
The difference is that APS considers the finite availability of your resources. APS checks several combinations of resources to find the fastest combination. The Pull Iterations planning parameter determines how many combinations to check. This planning method is much more realistic in that the system does not over-promise an order during a period when there are actually no available resources to complete the order. |
| No | Infinite APS calculates the lead time for the end item. To determine the start date, Infinite APS plans backward, starting at the due date, to the lead time value. Resources have infinite capacity. | No difference from Infinite APS. When APS plans an item that does not have a routing, the item is treated as if the MRP Item option (on the Items record) has been selected for that item. |
If, at any level of the BOM, the system cannot plan the operation with enough time remaining to plan all remaining previous operations, the pull-planning fails and the system instead push plans the entire demand (see About Push Planning for more information).
If the item being planned has a Time Fence defined, the pull-planning process includes additional steps. See Preserving Inventory and Supplies for Short-Term Demands for details.