Release Date

This field displays the selected item's release date. The system calculates the release date differently depending on whether you ran ran the Material Planner Workbench Generation with the Use Planned Data field set to Yes or No.

If Use Planned Data=Yes

If Use Planned Data was set to Yes when you ran the Material Planner Workbench Generation utility, the Release Date column will contain the release date calculated as follows, depending on the planning method you used:

Where:

FLT = Fixed Lead Time

VLT = Variable (per-piece) Lead Time

DTSLT = Dock-to-Stock Lead Time

PWLT = Paperwork Lead Time

If Use Planned Data=No

If Use Planned Data was set to No when you ran the Material Planner Workbench Generation utility, the system uses the following process to calculate the release date:

  1. The system determines the initial due date of the planned order. The due date is determined differently depending on the type of replenishment you are using on the Material Planner Workbench Generation form.

NOTE: For a description of these replenishment methods, see the Material Planner Workbench Overview help topic.

NOTES: