Reorder Point

This field applies to APS and only to purchased items that are neither MPS items nor Phantom items.

Reorder point items are usually inexpensive, high-volume items (such as nails, bolts, etc.) that you want to track and maintain differently than normal items.

If the Use Reorder Point field is selected, specify the inventory level that controls the point at which the system generates a planned order to replenish this item's on-hand inventory. When the on-hand level + the on-order quantity (total quantity from POs) drops to this reorder point level or below it, the system generates a planned order for the quantity specified in the Fixed Order Qty field. If that planned order quantity is not greater than the reorder point, the system uses the Order Multiple value to increase the planned order quantity until it is greater than the reorder point. If the Order Multiple value is zero, the Fixed Order Qty is used as the multiple to increase the planned order quantity. The system creates the reorder point planned order to be due at the current date + the item's lead time.

EXAMPLE: Consider the values below.

When you run the APS Planning activity, the system generates a planned order for 10.

NOTES:

Output Analysis

On the Planning Detail and Planning Summary forms and on the Exceptions Report, this field displays as a display-only reference. On planned orders for reorder point items, the Reference field displays "ROP" as a prefix to the PLN number and the Parent Reference field displays "Reorder Point."