Use Reorder Point

This field applies to APS and only to purchased items that are neither MPS items nor Phantom items.

Reorder point items are usually inexpensive, high-output items (such as nails, bolts, etc.) that you want to track and maintain differently than normal items. Select this field to specify that the system will replenish this item's inventory when on-hand inventory + on-order (such as from purchase orders) quantity drops below the level specified in the Reorder Point field. The system generates a planned order for the quantity specified in the Fixed Order Qty field.

Irrelevant Planning Parameters

Tracking reorder point items is a straightforward replenishment strategy for which many of the other planning parameters are not needed. When you select the Use Reorder Point field, the following fields on the Items form have no use and are disabled for this field.

CAUTION: When you select the Use Reorder Point field, the form sets the above fields to zero, if they contain a value, or clears them if they are selected (except the Accept Requirements field, which it selects automatically).

Output Analysis

On the Planning Detail and Planning Summary forms and on the Exceptions Report, this field displays as a reference.