Copy Routing BOM
	
	Use the Copy Routing BOM form to copy a 
	 routing and bill of material. You can select the source and target 
	 of the copy from:
	
		- The current bill of material
- Estimate jobs
- Jobs
- Actual jobs
- Production schedules
You can then edit the new copy of the routing 
	 and bill of material as necessary.
	
		NOTES:
		
			- If the source current routing/BOM contains alternate materials, 
			 they can be copied to the destination routing/BOM, depending 
			 on certain conditions. See "About Alternate Materials" 
			 in Copying 
			 Routings/BOMs for more information. MRP does not consider 
			 alternate materials; only APS uses them.
- When you copy materials to a job, if the target job (or 
			 estimate job) displayed in the To 
			 section of the form is a rework 
			 order (as indicated by the Rework 
			 field), you can copy a material to the job that is the same 
			 as the job's end item. This recursive BOM structure is allowed 
			 only for rework orders.
- You cannot copy a job structure to a new job if the job 
			 BOM contains a sub-job that is a rework order.
- You cannot copy materials from a rework order to a current 
			 BOM.
- The settings for the Preassign 
			 Lots and Preassign 
			 Serials check boxes on the original job are copied 
			 to the new job; however, any preassigned lot or serial numbers 
			 are not copied and must be generated for the new job.
 
	
Related Topics
Copying Routings/BOMs
Copying a Job with Configuration Information
Creating Routings and Bills of Material
Using Utilities and Activities