You can create a new routing and bill of material by copying it from another inventory item (which uses the current routing and BOM), another job, estimate job, or a production schedule item or release.
Use either of these forms to copy any type of routing/BOM.
Enter the appropriate data in the required fields. The From Category you select determines the fields you must enter.
Rework - If the displayed job is a rework order, the Rework field will be selected.
NOTES:
Copy Indented BOM - Default is No. Select Yes to copy the bill of material and create sub-jobs for any current subassembly materials within the BOM that have a Reference of Job.
NOTE: When you first create the sub-jobs in this manner, the Start and End dates on those jobs will be blank. The next time you run APS Planning, the system will populate these dates based on the current plan data. If you are using MRP, you must run Scheduling to populate the blank dates on the sub-jobs.
Select the Process button to start the copy process.
NOTE: If you set the Copy BOM field to Yes, and you are using the Infinite APS or APS planning mode, the message "[Planning] should be performed" displays. It is not necessary to run APS Planning immediately, but you should run it before the next time you run the Scheduling activity. The copy process may create sub-jobs with blank start and end dates; running APS Planning will populate those dates so the Scheduling activity can run properly. If you are using the MRP planning mode, the message "[Scheduling] should be performed" displays in this situation. With MRP mode, you must run Scheduling to populate the sub-job dates.
To copy an item's single-level current routing and BOM to the same item at other sites, see Copying a Multi-Site Item Bill of Materials.
The settings for the Preassign Lots and Preassign Serials check boxes on the original job are copied to the new job; however, any preassigned lot or serial numbers are not copied and must be generated for the new job.
The Job Orders and Estimate Job Orders forms allow you to create a new job or estimate routing by copying from the item's current routing. If you are copying from the item current routing, this method is easier than using the Copy Routing/BOM form.
NOTE: This method of copying the routing/BOM does not create sub-jobs for subassembly materials. You must use the Copy Routing/BOM form and enable the Copy BOM field to create sub-jobs automatically.
To update the planned material costs from the Items form, click Update Planned Costs.
This section applies only if you are using the APS planning mode.
The information below describes how alternate materials are copied when you copy the current routing/BOM in various forms in the system.
On the Engineering Workbench form, you can copy a material from a current routing/BOM to another routing/BOM. When you copy an alternate material in this manner, it is always copied to the new routing/BOM as a primary material. To make the material an alternate in the new routing/BOM, change the new material's Alt Group number appropriately before you save the new record.
When you copy a current operation from one item to another item, any alternate materials specified in the source operation are copied as alternate materials. However, when you copy a current operation to create any other type of operation (such as a job or production schedule operation), the alternate materials are NOT copied.
When you copy a current routing/BOM from one item to create a routing/BOM for another item, any alternate materials specified in the source routing/BOM are copied to the new routing/BOM as alternate materials.
When you copy a current routing/BOM to create another type of routing (such as a job or production schedule routing/BOM), the system copies any alternate materials APS selected in the last plan.
When you firm a job or production schedule release that APS has planned, and you copy the current routing/BOM, the system copies any alternate materials selected in that last plan. The alternate materials are copied to the new routing/BOM as alternate materials.
When you firm a job or production schedule release that has not been planned, and you copy the current routing/BOM, the system does NOT copy any alternate materials.