The combination of transfer orders and transfer order line items is used to control more formal movements of larger volumes of materials and items. This combination is characterized by:
A transfer order is used for the planning and controlling of stock movement and availability. When a transfer order requests that the material be transferred FROM the shipping site to the receiving site, the shipping site must be aware of this transfer order. If the material is being transferred TO the receiving site from the shipping site, the receiving site must be aware of this transfer order. After the transfer order is entered at one site, the system creates a complementary record automatically at the other site.
When you create the transfer order, the exchange rate defaults from the Inter-Site Parameters form, and cannot be changed. When adding or updating header information between two sites, the system determines whether the currency is different for each site. If so, the system stores currency in the domestic amount of the site.
When an item is produced at a remote supply site, the creation of a supply transfer order must trigger a demand transfer order at the supply site in order for the supply site to know about that order. With MRP or APS, you can set up replication to create a demand transfer order at the item's supply site. See Setting Up Planned Transfer Order Replication for more information.
With the APS Planning mode, you can also run APS Planning in global mode, which runs the planning program at each remote site in your supply chain. See About Global Planning for information about how global APS planning plans transfer orders. MRP does not support global planning.