Multi-Site Overview

The system allows you to perform the following multi-site functions:

About Sites and Entities

Logically, a site is any place where work is done. Thus, a site may correspond to company headquarters, a manufacturing plant, a distribution center, or a legal company that requires financial reporting.

Sites may report to financial reporting units called entities. An entity has a specific currency, a chart of accounts, and the ability to produce financial statements. For financial reporting purposes, you can assign sites to report to an entity. Sites can report to only one entity, and they must share characteristics with the entity such as account formatting, account numbers, and base (domestic) currency. For more information about setting up and using entities, see the Consolidation Overview.

Sites and entities are defined during database server installation, and additional information about each site and entity is set up on the Sites/Entities form. This information includes the intranet used by the site/entity and any linked sites. Replication rules may be set up to transfer data between sites, or master sites may be specified to maintain data for multiple sites.

Site groups may also be set up to combine data for sites performing related functions (for example, A/R payment generation or subcomponent manufacturing). Sites in a group do not have to be reporting to the same entity, but they do need to be sharing the appropriate data through replication.

You can add more sites later, as required by your situation. You can also create new entities, add a new site to an existing entity, and/or move sites from one entity to another.

Company Hierarchies

A corporate entity can have child entities (for consolidating reporting at different levels), and each entity can have child sites. Each site can contain multiple warehouses, and each warehouse can contain multiple item stockroom locations to store inventory.

The following chart shows the hierarchical relationship between components of a company.

hierarchical relationship between components of a company

Here, Sites A, B, and C are grouped to form Entity 1. There are two warehouses under Site A: Main and Dist. There are three locations shown under the Main warehouse: RAW1, FG2, and INS3.

Material Transfers Between Sites

There are two different ways to move or transfer items or material between SyteLine sites:

Both multi-site quantity moves and transfer orders support the use of lots and serial numbers.

Price Codes

The price code determines the costs that are used in multi-site quantity moves or transfer orders. You can set up price codes for sites that report to different entities. If both sites are in the same entity, price codes are not used.

Accounts

Multi-site transfer accounting automates inter-company financial transactions and inter-company financial consolidation. The system provides parameter set-up for profit/cost eliminations, and offers separate account tracking for inter-company profit, cost, Accounts Receivable, Accounts Payable, sales, and cost of sales.

Accounts must be set up to establish site relationships and default account numbers that will record inter-entity financial transactions. When initiating either a move or a transfer between sites, the costs and account numbers that default for the transaction come from the Inter-Site Parameters form and are relative to the site that initiated the transaction.

For more information,see About Multi-Site Transfer Order Costing.

Multi-Site Linked MRP and APS

SyteLine can replicate transfer orders between remote sites. When either MRP or APS creates planned transfer supply orders (PLNs) for components provided by remote supply sites, the planned transfer order is replicated to the supply site as a planned demand transfer order. See Setting Up Planned Transfer Order Replication for steps to set up this replication.

Demand and Source Vendor Sites

If you have separate demand and source vendor sites, with one site taking customer orders and maintaining POs while the other site fulfills those orders through a CO, you can set up a relationship between the sites to automate transaction processing. The process is similar to transfer orders but is between entities that are fiscally separate, so physical funds are moved through invoicing and vouchering. By automating the process, you can eliminate some of the manual data entry needed and ensure that the PO and CO remain in sync. For more information, see About Demand and Source Vendor Site PO-CO Automation.

Inter-Site Parameters

The Inter-Site Parameters form must be filled out prior to any A/P, A/R, or transfer multi-site activities taking place. These parameters establish the relationship between the sites ("inter" or "intra") and identify the inter-company accounts numbers to be used during transactions. If your sites are set up to replicate Site Admin data, you can enter these parameters in one site and all the others will update automatically.

Centralized and Decentralized Order Entry

If you want your sites to share customer order data, set up "centralized order entry" replication rules between the sites. This allows either:

When determining whether to implement centralized order entry, consider where Cost of Sales and Revenue are recognized. In centralized order entry, the shipping site incurs the cost and earns the revenue.

An order's shipment can span several sites: lines 1-3 are shipped from Site A, and lines 4-6 are shipped from Site B. Shipping and invoicing tasks must be performed at each shipping site.

Notes about multi-site customer orders:

Functions where Entity Data Is Not Available

Many system forms include a "Site" field that allows you to select a site. In some cases, both sites and entities are listed; however, if the data on the form is not applicable to entities, then only sites are listed.


Related Topics

Consolidation Overview

Adding a Multi-Site Item (No Master Site)

Adding a Multi-Site Customer (No Master Site)

Adding a Multi-Site Vendor (No Master Site)

Maintaining Items from a Master Site

Maintaining Vendors from a Master Site

Maintaining Customers from a Master Site

Creating Multi-Site Purchase Orders with the Purchase Order Builder

Moving Items or Materials Between Sites

Replication Steps

Setting Up Inter-Site Parameter Records

Setting Up a Master Site and Shared Tables

Default Replication Category Descriptions

Inter-Site Parameters

Multi-Site Quantity Move

Site Groups

Sites/Entities

Setting Up Inter-Site Parameter Records