About Multi-Site Transfer Order Costing

Transfer of material is supported through the use of transfer orders. Transfers can be made between warehouses within a site, between sites in the same financial entity, or between sites in different entities.

Transfer order header and line items are used to capture the information to drive the movement and costing of material. Once materials are transferred, transfer orders will create the necessary supporting accounting and material transactions.

Overview

Transfer Order costing will function in one of two ways depending on the setting of the Posting Method parameter, found on the Inter-Site Parameters form. The available Posting Method choices are:

Transfer Order processing first checks this Posting Method parameter to determine which types of financial entries to create. The actual scope of transactions created will also be affected by business processes at each site (for example, item cost at each site or pricing decisions).

CAUTION: No validation is provided to ensure that the system's financial environment does in fact exist as defined by this parameter. You are responsible for creating a financial environment that identifies how individual sites report financial results. The intent of the Posting Method parameter is to guide Transfer Order functionality in creating financial transactions that support a type of financial environment.

Costing and the Free On Board (FOB) Site

The designation of the Free On Board (FOB) point controls much of the supporting costing functionality. In the Transfer Order system, you can identify the FOB point as either the Ship Site or the Receive Site. You must specify the FOB point for all intercompany movements.

If the FOB point is the Ship Site, transfer of ownership takes place at the time of shipment. Material moves from a location in the Ship Site to a transit location in the Receive Site, and financial ownership changes from the Ship Site to the Receive Site. At receipt time, transactions are created to move the material from the transit location to a standard location at the Receive Site.

If the FOB point is the Receive Site, transfer of ownership takes place at the time of material receipt. Material moves from a location in the Ship Site to a transit location in the Ship Site. At receipt time, transactions are created to move the material from the transit location at the Ship Site to a standard location at the Receive Site. Financial ownership changes at receipt time.

When a site transfers inventory to another site, inventory cost at the shipping site is relieved against the five cost categories (Material, Labor, Fixed Overhead, Variable Overhead, and Outside Services).

When a site sells inventory to a site in another entity of the company, the Inter-Entity cost of goods sold at the shipping entity is debited against the five cost categories, and inventory is relieved against all five categories.

When a site receives inventory transferred from another site, inventory is received into stock as if it were a purchased item. If the receiving site has employed standard cost, the transferred item comes into inventory using the five cost elements (Material, Labor, Fixed Overhead, Variable Overhead, or Outside Services). If the receiving site uses any other cost type, the cost comes in as Material Only.

Supported Financial Transactions

Multi-site transfer order costing supports the following inter-site financial transactions:

Inter-Entity

NOTE: For Inter-Entity transfers, regardless of the cost method being used on the To Site, if the To Site cost is not equal to the From Site cost, then the difference is charged to inter-entity valuation variance.

Inventory Adjustment

Intra-Entity

Transfer Markups

The system supports two types of transfer markups:

Transfer Orders/Multi-Site Quantity Move and Costing

The method used to move inventory determines whether inventory moves through In-transit accounts or directly to the buyer's inventory accounts.

If you use the Multi-Site Quantity Move form, this method does not use the To and From Intransit Accounts of journal entries. However, if you use transfer orders, these can cause intransit entries to occur. The act of shipping and receiving inventory moves inventory into and out of Intransit accounts.

Examples

Following are specific examples of the multi-site transfer order costing methods in the system.

NOTE: The transfer process does not create journal entries if amounts or accounts are equal. Also, if items use standard cost on the receiving side, amounts are retained in separate cost buckets, as shown in most of the following examples. If items use actual cost, then all costs would be rolled into the material cost bucket.

Site to Site, Same Cost

Entity to Entity, Same Cost

Site to Site, Different Cost

Entity to Entity, Different Cost

Entity to Entity, Price Greater Than Cost

Site to Site, Same Cost, FOB Equals To Site

Entity to Entity, Same Cost, FOB Equals To Site

Site to Site, Different Cost, FOB Equals To Site

Entity to Entity, Different Cost, FOB Equals To Site

Entity to Entity, Price Greater Than Cost, FOB Equals To Site

Site A Actual Cost to Site B Standard Cost, Freight, Cost Markup

Site A Standard Cost to Site B Standard Cost, Freight, Cost Markup

Site A Standard Cost to Site B Actual Cost, Freight, Cost Markup

Entity 1 Site A to Entity 2 Site C, Cost and Profit Markup

Entity 2 Site C to Entity 1 Site A, Profit and Freight Cost Markup

Entity 1 Site A to Entity 3 Site D, Profit and Freight Cost Markup, Different Currency


Related Topics

Multi-Site Overview

About Transfer Order Costing

Inter-Site Parameters

Transfer Order Line Items

Transfer Orders