Transfer Orders Overview
		
	
		The combination of transfer orders and transfer 
 order lines is used to control more formal movements of larger volumes 
 of materials and items.
A transfer order is typically used for moving items 
 or materials between distribution centers, or for component and sub-assembly 
 movement between plants that require a more formal multi-stage transaction. 
 It does not require approval process or a requisition function.
Transfer orders are characterized by:
	- a transfer header and line items.
- picking process.
- separate entry of shipping and receiving transactions with provisions 
	 for recording loss, damage, rejects.
Transfer orders support the following:
	- visibility of in-transit inventory across the system including 
	 Transfer Order number, item, quantity in-transit, quantity to be shipped, 
	 date, shipment mode, freight cost, and value of shipment.
- financial transactions
- landed cost. All Landed Cost receipts must be vouchered before 
	 a transfer order can be closed.
- Cross-reference functionality.
- Picking List functionality.
- Packing Slip functionality.
- Bill of Lading functionality.
- Pro Forma Invoice functionality.
- various costing and pricing methods.
- automatic updating of inventory fields for Planned Transfer Orders.
- the ability to enter a transfer order without knowing the location 
	 or lot number. The location is not required until time of receipt. 
	 Likewise, if the receiving site enters the transfer order, it is not 
	 required to enter the from location of the items or materials being 
	 transferred.
- maintenance of the Transfer order header data from the shipping 
	 site when it creates the transfer order.
- partial shipping and receiving.
- ability to track quantity differences, such as: loss, shrink, damage, 
	 rejects, and advance shipment. These will be tracked by Reason Codes.
- Data Collection for shipping and receiving transactions.
Transfer Orders DO NOT support:
	- Change Order functionality.
- Configured Items.
- Discounts.
- Blanket Orders functionality.
- Progressive Billing.
- EDI functionality.
You can set up the system to replicate planned transfer order demand 
 orders to your remote supply sites (for MRP or APS Planning). See Setting 
 Up Planned Transfer Order Replication for more information.
Related Topics
Creating 
 Transfer Order Line Items
Creating 
 a Transfer Order Header
Setting 
 Up Inter-Site Parameter Records
Setting 
 Up Planned Transfer Order Replication
Transfer Orders 
 Steps
About 
 Currency Conversions for Transfer Orders
About Push/Pull 
 Transactions
About Transfer 
 Order Costing
About Warehouses
Transfer 
 Order Status Report