Creating a Transfer Order Header
	- Open the Transfer 
	 Orders form.
- Select Actions > New.
- Enter the appropriate data in the required fields. 
	
		- Transfer - Enter a unique 
		 identifier composed of numbers, characters, or a combination. 
		 You can set the global prefix, Transfer Prefix, in the 
		 Transfer 
		 Order Parameters form. This prefix starts all generated 
		 transfer numbers with the same prefix followed by a system-generated 
		 number.
- Status - Enter a status or 
		 accept the default, which is Ordered. The options are: 
		 
		
- From Site - Enter the site 
		 from which to transfer the inventory.
- To Site - Enter the site 
		 to receive the inventory.
- From Whse - Enter the warehouse 
		 from which to transfer the inventory.
- To Whse - Enter the warehouse 
		 to receive the inventory.
- # Packages - Enter the number 
		 of packages associated with this transfer. This field can be used 
		 to record the number shipped and then to validate the number received.
- Tot Weight - Enter the weight 
		 of this transfer. This information is helpful to verify against 
		 the bill that will be supplied by the shipping vendor.
- Ship Via - Enter the code 
		 which tells the shipper how you would like this transfer order 
		 shipped.
- EU VAT fields - If necessary, enter EU VAT information (NOTC, 
		 Delivery Terms, and so on).
 
- Select Actions > Save.
- If there are associated landed costs, to set them up on the Transfer 
	 Order Landed Costs form, click the Landed Costs button.
- To add line items, you can click the Lines button to open 
	 the Transfer 
	 Order Lines form. For more information, see Creating 
	 Transfer Order Lines.
Related Topics
Transfer 
 Orders Overview
Transfer Orders 
 Steps
Transfer Orders 
 Steps