To configure an Estimate Job, do the following:
NOTE:When you are in a configuration session, the system prevents you from accessing any SyteLine forms or online help.
After processing, the system updates the Estimate Job Orders form with the configuration information.
For a configurable job/item with an incomplete configuration, or which has not been configured at all, the Configure button remains enabled.
When a configuration is complete, the Configure button changes to Configure-Complete.
If Auto Job Generation is set to Always for this item on the Items form - Configuration tab, a cross-reference job is automatically created.
If Auto Job Generation is set to Prompt, the system asks if you want to create a cross-reference job.
Rules can be defined that place anInfor Product Configuration Management configuration on hold if, for example, an option in the configuration requires approval. When the original user completes the configuration, the Configure button for the line is set to Configure-HOLD, and the Config Hold field is selected. When a configuration is approved, you can either reconfigure the estimate job to remove the hold in Infor PCM, or you can select the Actions>Remove Config Hold menu option in SyteLine. The button label is updated to Configure-Complete and the Config Hold field is cleared.
The configuration hold extends to any sub-jobs. Those sub-jobs cannot be released until the hold is removed.
Attaching Infor PCM Documents to SyteLine Records
Copying a Job with Configuration Information
Deleting Configurable Jobs, Items, and Operations
Printing Configuration Information
Reconfiguring a Line Item or Job
Setting Up a Configuration Interface for an Item or Job - Infor PCM