An estimate job contains information about the item being quoted, including quantity required and scheduled completion. However, it is not included in actual Shop Floor production schedules. Use the Estimate Job Orders form to create an estimate job.
Status - Select a status or accept the default of Working. Options are:
Start Date - Enter the start date for the estimate job. The End field is the date by which it should be completed. The Start date is required; the system calculates the End date when you save the job. The Projected date is entered automatically when you click the Get ATP or Get CTP button or when you run the Planning or Scheduling activities.
NOTE: If the start or end date falls on a weekend and Saturday and Sunday are not defined as manufacturing days, the system adjusts the date to reflect a weekday.