Creating and Entering a Planning Item

NOTE: This topic applies only to the Features and Options Product Configurator.

Design the Planning Item Layout

On paper or a spreadsheet, design the layout of the planning item you wish to create. The layout should include the following:

Create the Feature Groups

Features groups are used to tie inventory items in a bill of material together, grouping like or similar types of material.

  1. Access the Feature Groups form.
  2. Create a new group and enter the appropriate data in the required fields:
  3. Select Actions > Save to save the record.
  4. NOTE: When entering the qualifier mask use . (periods) for spaces and X's for characters. An * (asterisk) can be used as a wildcard for all the other feature codes to the right.

Create Feature Group Qualifiers

Create the feature group qualifiers. The feature group qualifiers are the actual codes that will be used to describe each choice of the inventory items of a feature group.

  1. Access the Feature Group Qualifiers form.
  2. Select the appropriate feature group.
  3. Add a new qualifier record and specify this information:
  4. Select Actions > Save to save the record.

Create All Inventory Items Needed for the Planning Item

Update the Items form to reflect that this item is a planning item. Any item that has the Configuration Flag selected at any level in the BOM must also have the Configuration Flag field selected at the end-item level.

  1. On the Items form, create the inventory item.
  2. Select the Configuration Flag field to indicate that this item is a planning item.
  3. After creating the inventory item, you must create the bill of material. The Current Materials form required fields are:
  4. If the individual inventory items, also referred to as components, are not lot or serial tracked, make sure these features are turned off. You can turn off lot or serial tracking at the individual item level on the Items form's Controls tab.

    NOTE: If lot or serial tracking is done at the individual inventory item level, you will be prompted to enter the required information for each item when inventory is impacted.

Create the Feature Group Rank

The feature group rank tells the features-and-options product configurator which feature groups are being used for this planning item. This step will need to be executed for all BOM items which contain sub-planning.

  1. Access the Feature Group Ranks form.
  2. Find the correct inventory item to rank.
  3. Select the Generate button to generate the ranking.

Related Topics

Features-and-Options Product Configurator Steps

Adding a Configured Item in Order Entry

Example: Setting Up a Configured Subassembly