Example: Setting Up a Configured Subassembly
NOTE: This topic applies only to using the Features
and Options Product Configurator.
In this example, you will add a wheel to the current BOM of FO-10000,
and allow customers to choose the color of the wheel reflectors.
- Open the Copy Items activity and copy the following items. Be sure
to select the checkbox to copy the Current BOM.
- SA-61500 to SA-61700
- RF-30000 to RF-30100
- RF30000 to RF-30200
- Open the Items form and update the desctiptions of the new items.
- SA-61700 - "CONFIGURED SUBASSEMBLY"
- RF-30100 - Add "WHITE to the end of the description
- RF-30200 - Add "YELLOW" to the end of the description
- Update SA-61700.
- Deselect the Stocked checkbox so that cross-referencing will
create a configured sub-job for the wheel.
- Make SA-61700 a configured item by selecting its Configuration
Flag checkbox.
- Update feature templates.
- Update the FO-10000 feature template to include the wheel and
reflectors by adding two segments to the end of the template.
The final template should be "&&-&&&-&&&-&&-&&".
- Enter the same template on SA-61700.
- Create feature groups.
- Wheel
- ID: TWHEEL
- Description: wheel
- Mandatory: Yes
- Mask: two characters at positions 9 and 10 (........XX*).
- Reflectors
- ID: TREFL
- Description: reflectors
- Mandatory: Yes
- Mask: two characters at positions 11 and 12 (..........XX*).
- Create feature group qualifiers.
- For the wheel option
- Feature: TWHEEL
- Include: Yes
- Code: "........SA*
- For the white reflector option
- ID: TREFL
- Include: Yes
- Code: "..........WH*
- For the yellow reflector option
- ID: TREFL
- Include: Yes
- Code: "..........YL*
- Update BOMs.
- SA-61700
- Add a quantity of 2 RF-30100 and a quantity of 2 RF-30200
to operation 10.
- Link both materials to the new feature group and fill in
the appropriate Option Code.
- FO-10000
- Add a quantity of 2 SA-61700 to operation 10.
- Verify that Reference = Job. If you fail to do this, the
system will not create sub-jobs and BOMs when you create the
cross-references.
- Generate feature group ranks.
- For SA-61700.
- For FO-10000, make sure you re-rank the seat before the rack.
- Add a new customer order line for FO-10000 and verify the subassembly
features and options are visible and updating the config string appropriately.
- Save the line and click Source to generate the job orders and configured
BOMs for FO-10000 and SA-61700. Verify that the correct jobs and BOMs
were created.
Related Topics
Creating
and Entering a Planning Item
Features-and-Options
Product Configurator Steps