Creating Costing Alternatives

To create a costing alternative:

  1. Open the Costing Analysis Workbench form. It can be accessed from the Controller Home form or SyteLine Explorer.
  2. Click New.
  3. Specify this information:

Copy Routing is typically used to create a year-end snapshot of rates for history or to analyze detailed changes to the current BOM and routing. Do not copy the routing if you want to selectively change items’ labor, material, and/or overhead rates, and then use your changes to update master records.

  1. On the SyteLine toolbar, click Save. After you save this record, you cannot change these values. To make changes, you must delete the record and start again.
  1. The next step is to add items to your costing alternative, which you can freeze or for which you can change various costing rates for analysis. You can click Copy Costing to add groups of manufactured items using the Costing Analysis Alternative Copy form. You can also use  the Items tab on the Workbench to add individual items. If you use the copy form, then after you process the copy, return to the Workbench and refresh the record to see added items. Following are several guidelines for adding items:
  1. After adding items, save the record.
  2.  Do one of the following:
  1. The next step is to roll up new item costs for the changes you have made. See Rolling Up Costs for Costing Analysis.

Related Topics

Costing Analysis Overview

Rolling Up Costs for Costing Analysis

Comparing Costs for Costing Analysis