Comparing Costs for Costing Analysis

The Compare tab on the Costing Analysis Workbench is used for comparing costs for costing analysis. A rolled up costing alternative record can be compared with items' current or standard costs, or with costs in another costing alternative.

To compare costs:

  1. Open the Costing Analysis Workbench form and select the costing alternative record for comparison.
  2. Click the Compare tab. The selected costing alternative is displayed on the left side of the form.
  3. On the right side of the form, do one of the following:
  1. In the middle of the form, select an item in the grid. Comparison data for the item is displayed on the tabs at the bottom of the form:
  1. You can make additional changes to the costing alternative as needed for your analysis.

If this analysis is for a costing alternative that did not use a copied routing, and if your analysis shows that the revised rates are where you want them, the next step is to roll the rates to current using the Costing Analysis Alternative Roll Costs to Current form. See Costing Analysis Alternative Roll Costs to Current.


Related Topics

Costing Analysis Overview

Creating Costing Alternatives

Rolling Up Costs for Costing Analysis