Adding Routing/BOM Information with Engineering Workbench
You can use Engineering 
 Workbench to add a routing and bill of material to inventory items 
 (the current routing), jobs, production schedules, or estimate jobs.
Selecting the Transaction
	- In the View field, select the type of routing/BOM: current (inventory 
	 item), standard, job, estimate, or production schedule.
- Click the filter button in the toolbar.
- Use the header fields to select the item, job, or production schedule 
	 to which you want to add routing/BOM information.
- Click the filter button again. Any existing routing information 
	 for the item, job, or schedule is displayed.
Creating the Routing
	- In the Operations grid, add a new record for each new operation 
	 in the routing. Use the grid fields to select a work center and define 
	 operation setup, queue, and run times, as well as the start and end 
	 date and other information about the operation.
- After adding all the operations for the routing, select Actions 
	 > Save.
- If you need to define resources for an operation beyond the default 
	 resource group defined for that operation's work center: 
	
		- Right-click on the operation number in the Operations grid 
		 and click Details. The appropriate Operations form opens, 
		 with the record for this operation displayed.
- In that form, select the Resources tab and define the crew 
		 or machine resource groups that this operation requires in order 
		 to be processed, as well as parameters related to the resource 
		 groups.
- Save the record and close the form.
 
- If you need to define costs for an operation: 
	
		- Right-click on the operation number in the Operations grid 
		 and click Details. The appropriate Operations form opens, 
		 with the record for this operation displayed.
- In that form, select the Costs tab and define the values used 
		 in costing this operation.
- Save the record and close the form.
 
Adding Materials
The Engineering Workbench record containing a new operation must be 
 saved before you can add materials for the operation.
	- In the Materials grid, add a new record. Select an operation for 
	 which you want to define a material. Then select or enter the rest 
	 of the information about the material. You can add multiple lines 
	 defining different materials for a single operation.
- Once you have added all the materials for the operations you defined, 
	 select Actions > Save to save the new materials.
Viewing the New Routing/Materials in the Left Tree Pane
The left pane of the Engineering Workbench form contains 
 a tab for each of the following routing/Bills of Material (BOM):
	- Current
- Standard
- Job
- Estimate
- PS Item
- PS Release
To see in the left pane the new operations or materials you added, either 
 close and reopen the Engineering Workbench form, or click the filter button 
 on the left pane and click OK in the dialog that appears. Either 
 method refreshes the tree pane.
The tree display is shown here:

You can collapse the tree display into a simpler view 
 by selecting the (-) symbol next to each item or operation. For example, 
 suppose you want to look at operations for the item, without displaying 
 the materials. Click the (-) symbol next to the operation, and the materials 
 disappear in the collapsed tree. The word "Alternate" appears 
 next to any material that is specified as an alternate 
 material on a current operation.
NOTE: You cannot 
 add or remove operations or items from routing/BOMs in the left pane. 
 Use the right pane of the Engineering Workbench form for maintaining 
 routing/BOMs.
Related Topics
Creating 
 Routings and Bills of Material
Engineering 
 Workbench