Displaying Demand Records

To determine which demands display on the Demand Summary APS and Demand Summary - Scheduler forms:

  1. Ensure that Filter-in-Place is activated.

  2. In the header section, use the Start Date and End Date fields to select the starting and ending dates to define the period you want to analyze. Only demands with a Due date, Start date, End date, or Scheduled date within this date range will be displayed in the results grid. Leave the Start/End Date blank to use the default date specified in the Days to Schedule field on the Shop Floor Control Parameters form.

  3. In the grid, use the Type, Demand ID, Item, and Days Late fields to further filter the demands that will display.
  4. Deactivate Filter-in-Place.

NOTE: When filtering by Demand ID, you must also enter a Type. Enter the Type first and then select the Demand ID on which to filter. The system uses the combination of the Type and Demand ID to filter the results.

NOTE: When filtering by Days Late, enter the > symbol and a number of days late to limit the display; for example, enter >5 to display all demands with lateness greater than 5 days.


Related Topics

APS Overview