APS Overview
The Advanced Planning System (APS) generates real-time projections of 
 when you can complete orders by comparing all demands (such as customer 
 orders) against a long-term plan. The system views the current status 
 of inventory levels, forecasts, job schedules, PO due dates, customer 
 orders, etc. and creates planned orders accordingly to satisfy 
 the demands. You then "firm" the planned orders into purchase 
 orders, purchase requisitions, job orders, production schedules, or transfer 
 orders.
The long-term plan includes information such as:
	- Demand orders that consume inventory and resource capacity
- Supply orders that add to inventory
- Each operation in the plan
- Each item in the plan
- The projected completion date for every planned order
- Each resource allocated to a job
- Scheduled operations (for work orders in which the resource usage 
	 is frozen)
- Every lateness cause for every demand in the plan
Modes of APS Planning
Infinite APS vs. APS
You can run the planning system in Infinite 
 APS mode or APS 
 mode. The difference between these modes of planning is in the resource 
 capacity the system considers when generating a plan. Infinite APS assumes 
 infinite 
 resource capacity, while APS constrains the plan realistically based 
 on availability of resources.
	- APS mode considers whether the crew and machines are on-shift and 
	 not busy working on another demand. In APS, resources are capable 
	 of working on a limited number of tasks while on shift. In APS mode, 
	 the Get 
	 CTP button is available on various forms such as Customer Order 
	 Lines and Job Orders.
- Infinite APS mode uses the sum of the Move, Queue, Setup, Run, 
	 and Finish times defined for the operations and assumes the resources 
	 are capable of working on an unlimited number of tasks while on shift. 
	 In Infinite APS mode, the Get 
	 ATP button is available rather than the Get CTP button.
See Resource 
 Planning Examples for an illustration of how Infinite APS and APS 
 plan resources for the same order data.
See About 
 the APS Planning Process for a detailed discussion of how the APS 
 algorithm plans demands into available supplies, on-hand inventory, and 
 resource capacity.
	NOTE: If the APS module is unlicensed, 
	 APS Planning can only be run in Infinite mode. 
	
	
	
Material 
 Requirements Planning(MRP) plans requirements for items according 
 to the level the item appears in a BOM, batching together requirements 
 needed at the same period of time. Like APS, MRP generates planned orders, 
 which you firm into actual SyteLine 
 transactions.
MRP and APS use the same basic input data. However, the APS system plans 
 all requirements for one demand (through the end item's entire BOM), then 
 plans all requirements for the next demand, and so forth for all the demands, 
 based on order priority and each demand's due date.
Examples of APS differences from MRP are as follows:
	- APS "pull-plans" 
	 each demand backward in time, starting from the due date, to determine 
	 the start dates for the planned orders. If any single component from 
	 the demand cannot be pull planned within the time between the due 
	 date and the current date, the system "push-plans" 
	 the entire demand forward in time, starting from the current date, 
	 out to an as-soon-as-possible date. APS never plans into the past 
	 (unlike MRP, which allows start dates in the past).
- APS does not automatically combine planned orders for items that 
	 are needed within the same period of time. You can set the Planned 
	 Orders Consolidation options on the Advanced tab of the Planning Parameters 
	 form if you want planned orders to be combined, such as for a "days 
	 supply." See Consolidating 
	 Planned Orders for more information.
- APS does not always recommend moving a job to an earlier date to 
	 satisfy a demand. Instead, it creates a new planned order due earlier 
	 than the existing firmed job. However, if the supply is available 
	 within the Supply 
	 Usage Tolerance, the system will use the supply when the demand 
	 needs it. This behavior is appropriate in a finite capacity environment 
	 because you may be able to feasibly fit in a small job for a small 
	 order in situations where a larger job could not be moved.
Setup Steps and Daily Procedures
	- See the Infor SyteLine Installation Guide 
	 for installation and setup procedures related to APS.
- See APS Steps 
	 for the general business process and related procedures.
Methods of Planning
You run APS in the following situations:
	- APS Planning form: When you initially set up the system, and then 
	 on a scheduled basis (such as nightly), you run APS Planning to synchronize 
	 all demands with the latest inventory, supply, shifts, and resources 
	 information. You can run APS Planning for a single site or globally 
	 across all sites defined on the APS 
	 Sites and Alternate Management form. You can also set up the system 
	 to replicate 
	 demand transfer orders to your supply sites. 
	The system deletes all existing plan information and regenerates 
	 it using the latest data. In most situations, you will run APS Planning 
	 for a long horizon, such as one or two months. (If you are using Scheduling, you 
	 will likely run the Scheduler with a shorter horizon, such as one 
	 or two days.) The APS Planning activity creates planned orders and 
	 exception messages. 
- Incremental planning: When you save certain types of transactions 
	 (such as customer orders and job orders), AND the Plan 
	 on Save field is selected on the transaction, SyteLine inserts 
	 the new demand into the existing APS plan. The demand is planned using 
	 the inventory, supplies, and capacity that were not allocated to other 
	 demands during the last run of APS Planning or by demands that were 
	 previously incrementally planned. See About 
	 Incremental Planning and ATP/CTP for more information.
- Get ATP/CTP: For certain transaction types, the system can insert 
	 a single demand/line item into a temporary "test" copy of 
	 the plan to determine feasibility. In Infinite APS mode, the resulting 
	 availability date is referred to as the available-to-promise (ATP) 
	 date. In APS mode, it is the capable-to-promise (CTP) date. The ATP/CTP 
	 process returns a projected availability date for the demand; if the 
	 date is acceptable, you can allow the system to insert the demand 
	 incrementally into the actual plan.
Planned Orders and Interaction with the Scheduler
When you run APS Planning, the system creates planned orders for demands 
 that were not satisfied by on-hand inventory and planned supplies. On 
 the Shop 
 Floor Control Parameters form, you can specify that the Scheduler 
 consider these planned orders as demands that must allocate resources 
 (thus creating a more realistic scheduling simulation).
After you firm 
 the planned order into a job, purchase order, etc., you can run APS 
 Planning again to plan the new demand (using its routing/BOM). When you 
 then run the Scheduler, the operation start and end dates are based on 
 the dates APS calculated for the original planned order (the operation 
 start and end dates may change depending on the rules set up for the Scheduler). 
 Subsequent runs of APS Planning will treat those scheduled operations 
 as "frozen," and will not move the operation start and end dates. 
 However, subsequent runs of the 
 Scheduler may move the operation start and end dates again based on the 
 latest information.
Related Topics
APS Steps
Analyzing 
 APS Output
Consolidating 
 Planned Orders
Controlling 
 Planned Order Creation
Creating 
 APS Alternatives
Creating 
 Outside Operations
Defining Lead Time 
 for APS Planning
Defining 
 Overlapping Operations
Defining the 
 Work Week
Planning 
 a Job's Operations
Refreshing 
 the APS Plan to Reflect Changes
Running APS 
 Planning
Setting 
 Up Planned Transfer Order Replication
Troubleshooting 
 APS
Using 
 Lot Sizes with MRP and APS
Using 
 Supply Usage Tolerance
Writing 
 a Custom Operation Calculation
APS Order Priority
APS Planning
About Exception 
 Messages
About 
 Global Planning
About Incremental 
 Planning and ATP/CTP
About Job Dates
About 
 Operation Run Time - Planning and Scheduling
About 
 Phantom Items in MRP and APS
About 
 the Planning Process
Defining Lead Time 
 for APS Planning
Demand Summary 
 APS
Demand 
 Detail Chart APS
Examples: 
 Resource Planning
How 
 APS Interprets Job Status
Material 
 Planner Workbench
Operation 
 Setup Time Overview
Order Action 
 Report
Planning Parameters
Resource Gantt 
 Chart
Resources Overview
Scheduling 
 Overview
Using APS to 
 Backward Schedule
Filtering 
 APS Messages