Firming Planned Orders into Job Orders
When the Source field on the General
tab of the Items
form is set to Manufactured and the Production Type on the
Planning tab of the Items form is set to Job, the
system firms each selected planned order into a new job.
- From the Planning
Detail form, select the planned order(s) you want to firm.
- Click the Firm button. The system displays the Planning
Detail Firm Job form.
- In the Job Prefix field, perform one of the following actions:
- To use the default prefix defined in the Shop
Floor Control Parametersform, leave the field blank.
- To use a prefix other than the default, enter a different job
prefix.
- If you want the system to create a single-level job, select Copy
Current BOM.
- If you want the system to generate orders for any associated sub-jobs
as well as the top level jobs, select Copy Indented BOM.
- Click OK.
The system firms the planned orders into new jobs, assigning the
next available job numbers.
NOTE: The system
creates the job header automatically, but you must either copy
or create the routing and bill of material.
Related Topics
Firming Planned
Orders
Firming
Planned Orders into Transfer Orders
Firming
Planned Orders into a Purchase Order
Firming
a Planned Order into a Production Schedule
Planning Detail