When the Source field on the General tab of the Items form shows that the source of this item is Purchased and the Create PO Reqs from PLN field in the Planning Parameters form is cleared, the system firms each selected planned order into lines or releases on a purchase order.
To firm multiple orders at once, use the Material Planner Workbench.
The system displays the Planning Detail Firm PO form.
If you select a regular PO, the planned orders become lines on the PO. If you select a blanket PO, the planned orders become releases on the PO.
NOTE: If you enter an existing blanket PO, and this item does not appear on any line in the PO, the system sums the quantities of the selected planned orders and stores them in the newly created blanket PO line.
If you entered an existing PO number, the vendor for that purchase order displays automatically in the Vendor field.
NOTE: For existing purchase orders, the system always uses the vendor specified on the purchase order, rather than the default vendor from any existing item/vendor cross-reference.
If the parameter is set to Always, the system creates the PO change order automatically.
If the parameter is set to Never, the Perform Change Order field is disabled.
NOTE: If you leave the Vendor field blank, the system assigns the item's first-ranked item/vendor cross-reference. If no item/vendor cross-reference exists, the system creates the PO with no vendor assigned.
Firming Planned Orders into Job Orders
Firming Planned Orders into Transfer Orders