Firming Planned Intra-Site Transfer Orders
To firm planned intra-site transfer orders:
- On the
Intra-Site Transfer Detail form, select the planned intra-site
transfer orders to firm. These orders have a reference ID that begins
with TPLN WTD.
- Click Firm. The Intra-Site
Transfer Detail Firm Transfer Order form is displayed with
values set for the From and To sites, and From and To warehouses as
defined on the planned intra-site transfer orders.
- In the Transfer field, do one of the following:
- To let the system assign the next available transfer number,
leave the field blank.
- To use a prefix other than the default, specify a new transfer
prefix.
- Select an existing transfer number. Only transfer orders for
which the From and To Warehouses match the corresponding warehouse
values for the planned intra-site transfer orders are displayed.
The planned orders become lines on the existing transfer.
- Click OK. The system firms the planned intra-site transfer
orders into the new or existing transfer order, and the planned intra-site
transfer orders are replaced with a reference to the new or existing
transfer order line.
Related Topics
About Intra-Site
Transfers
Intra-Site
Transfer Setup, Planning, and Review