Handling Resource Reallocation During Interruptions
When the Scheduler is processing a load of items on 
 a job, it usually completes an operation and moves on to the next one 
 in the routing. However, certain situations can interrupt the load from 
 being processed at an operation:
	- End of a shift
- Start of a shift exception
- Start of a holiday period
Three things happen when the load is interrupted:
	- Operation processing for the load stops.
- The resources that have gone off-shift become unavailable.
- All other resources allocated to the load remain allocated.
The system keeps track of each unavailable resource for the load. Once 
 interrupted at an operation, a load must wait to resume operation processing 
 until the system can again allocate all of the load's needed resources.
Setting Options to Handle Interruptions
You can set options to handle load interruptions as follows:
	- Process the load on a substitute resource.
- Reserve the current resource (the one that is now off-shift).
- Place the load back into the resource's request queue.
Use the Reallocate 
 option on the Resource Group and the Allocation 
 Type on the Resource to control interruptions. The diagram below illustrates 
 the combinations of the two options:

	- Reallocate selected: The load frees the resource and tries to reallocate 
	 a resource from the same resource group. Any member of the resource 
	 group may serve as a substitute for the unavailable resource on this 
	 operation. The Scheduler does not consider the permanent/temporary 
	 state of the resource if Reallocate is selected on the resource group.
- Reallocate not selected: The load can wait until that specific 
	 resource is available. The setting of the original resource's Allocation 
	 Type determines whether the load reserves that resource or must compete 
	 with other loads to reallocate it.
- Allocation Type=Permanent: To resume processing at the operation, 
	 the interrupted load must regain the unavailable resource. It cannot 
	 allocate any other resource, and only this load can allocate the resource. 
	 Reallocation takes place when the resource becomes available, whether 
	 reallocation of any other needed resources succeeds or fails.
- Allocation Type=Temporary: The interrupted load must regain the 
	 unavailable resource to resume operation processing. No other resource 
	 can substitute. The interrupted load must compete with other loads 
	 for the unavailable resource when it becomes available. The system 
	 places the load in the resource's request queue. Reallocation occurs 
	 only when the needed resource becomes available and when the interrupted 
	 load's request is selected.
NOTE: If one or more 
 of the needed resources belongs to a resource group that has the Reallocate 
 field cleared, reallocation is not possible until those resources become 
 available again.
You will usually enable the Reallocate field for groups that contain 
 labor resource types working on different shifts, but not for machine 
 resource types.
Related Topics
Resource Groups
Resources