Resource Groups

This form is used only with the APS planning mode and the Scheduler.

Use a resource group to organize resources that can perform the same function. Then, when you create an operation, you specify one or more resource groups to process the operation. When a load of items from a job arrives at the operation to be processed, it requests one or more resources from each of its specified resource groups. It does not need a specific resource in the group. The member resources may be working different shifts, have different setups, or have different processing times.

You cannot use a resource group on an operation unless it has at least one resource assigned to it.

NOTE:Resource groups have replaced the work center's scheduling functions as they existed in SyteLine version 6 and earlier. The work center now captures costs only and does not affect the actual planning or scheduling.

The Where Used report is accessible from the Actions menu. It displays the items, jobs, and work centers that reference this resource group.

How the Scheduler Assigns Resources

The Scheduler assigns an available resource to the load based on allocation rules you define (such as "choose the resource that has been idle the longest"). Depending on the allocation rules defined, various factors may affect how the Scheduler selects one of the member resources over the others. The Seq field on the Resources tab is important, especially when using The "Select in Sequence" and "Cyclic" Allocation Rules because they allocate the resource with the lower Seq value first.

See Using Scheduler Rules for more information.

How APS Assigns Resources

APS selects resources from the resource group based on the best combination of resources from all resource groups required for the operation. In this case, "best" means the combination that allows the operation to be planned the fastest.

For example, an operation may require 1 resource from labor resource group "Drillers" and 1 from machine resource group "Drill." Each of these resource groups contains five resources that could do the work. The system starts at the top of the list of resources defined for each group and, for each resource, examines information such as shift availability and whether the resource is already busy on other jobs.

The Seq field on the Resources tab is important because it determines the sequence of the resource list and can affect which resource the system chooses in the case of "ties."

See About the Planning Process for more information.

How to Assign a Specific Resource

To assign a specific resource to work on an operation, create a resource group that contains only that resource. On the Operation record, reference that resource group on the Resources tab.


Related Topics

APS Overview

Resources Overview

Scheduling Overview

About Infinite Resource Capacity

Analyzing Scheduler Output

Current Operations

Handling Resource Reallocation During Interruptions

Items

Job Orders

Resources

Scheduling Shifts

Work Centers