Follow these steps to implement either LIFO or FIFO inventory cost method:
NOTE: When the beginning inventory balance is entered by way of a stock adjust transaction, a record is created in the Item LIFO file with the current date, time, quantity, and the cost that is entered. If an item has no beginning inventory balance, leave a zero in each of the Unit Cost Detail fields and a LIFO/FIFO stack will be created as the item is received into inventory.
If you have entered Actual in the parameter default Cost Type field, and selected the Post to Journal check box to indicate that the manufacturing modules are to post inventory transactions to G/L, you must also set up the G/L account numbers that the system uses for this interface. Listings of the account numbers and related codes and parameters which need to be entered for costing purposes follow.
WIP Material
WIP Labor
WIP Fixed Overhead
WIP Var. Overhead
WIP Outside Services
Inventory Adjustment
Matl Fovhd Applied
Matl VOvhd Applied
NOTE: The Fixed Material Overhead Applied and the Variable Material Overhead Applied accounts are required only when overhead is based on job material issues.
Fixed Ovhd Applied Acct
Variable Ovhd Applied Acct
Direct Labor Applied Acct
Fix Mach Ovhd Applied Acct
Var Mach Ovh Applied Acct
Inventory Material
Inventory Labor
Inventory Fovhd
Inventory Vovhd
Inventory Outside
COGS Material
COGS Labor
COGS Fovhd
COGS Vovhd
COGS Outside
In-Transit Material
In-Transit Labor
In-Transit Fovhd
In-Transit Vovhd
In-Transit Outside
NOTE: You are allowed to delete any distribution account record, including the default distribution account with a blank warehouse and blank Product Code.
About Posting - LIFO and FIFO Cost Methods
How LIFO/FIFO Stacks Function When Using Item/Warehouse Costing