Tracking Lot-Controlled Materials
You can trace lot numbers through multiple transaction or job levels. 
 You can trace lots forward, to determine the ultimate item in which a 
 lot-tracked item is included.
Using the Lots Form
To trace lots:
	- On the Lots form, specify 
	 the item and lot number to trace.
- Select the Lot Trace tab. The tab displays the root node of a tree.
- Click on nodes to expand the information. The tree initially shows 
	 the source transaction of the lot/item. If that transaction is a job, 
	 the tree includes additional nodes for any lot/item materials in that 
	 job, as well as nodes for the source of those lot/items. 
- Continue through the nodes until there are no more job sources, 
	 or job sources with lot item materials. 
Using the Lot Traceability Report
To trace lots:
	- On the Lot Traceability Report 
	 form, specify the range of items and lot numbers to include.
- In the Summary or Detail 
	 field, specify: 
	
		- Summary to show only 
		 the immediate source transaction.
- Detail to show the 
		 detail of source jobs, where those jobs contain lot items that 
		 themselves have a source. Additional levels are indented on the 
		 report. 
 
- Click Print.
Multi-Site Transfer Orders
For information about moving lot-tracked transfer orders between sites, 
 see About 
 Multi-Site Transfer Order Lot Tracking. 
Related Topics
Preassigning Lot Numbers
Defining Intelligent Lot and 
 Serial Numbers
About 
 Multi-Site Transfer Order Lot Tracking