Defining "Intelligent" Lot and Serial Numbers with Prefixes
You can assign prefixes to lot and serial numbers that include variable
information such as the current month/day/year, the site, the reference
type/number/suffix, and/or a literal value, as well as any constant values
you specify.
You can also still type in a standard prefix such as "SN-".
Maximum size for lot numbers, including the prefix, is 15 characters.
Maximum size for serial numbers, including the prefix, is 30 characters.
Defining an Intelligent Lot Prefix
To define an intelligent prefix to use with lot numbers:
- Click Lot Definition on
one of these forms:
- For a global lot prefix that applies to all items, click Lot Definition on the Inventory
Parameters form.
- For a lot prefix that applies to a specific item, click Lot Definition on the Items
or Multi-Site
Items form. This prefix overrides any global lot prefix.
- On the Prefix
Definition form, add a line for each segment of the prefix.
- To specify the segments of the prefix:
- Click in the Segment Value
field and select from the list of placeholder options. See the
table below for explanations of the options.
- You can include as many segments as you need in the prefix.
However, the lot length is limited to 15 characters. If
you specify a prefix that could be greater than or equal to the
limit, you receive a warning.
- To include a constant, for example a hyphen, specify Constant in the Segment
Value field and then specify the character(s) in the Segment Placeholder Value field.
- To change the order of the segments, click the Up
and Down buttons.
- The full prefix (using placeholders) is displayed in the Prefix field.
- Click OK to return to the
previous form, where the prefix is displayed in the Lot
Prefix field.
Defining an Intelligent Serial Number Prefix
To define an intelligent prefix to use with serial numbers:
- Click S/N Definition on
one of these forms:
- For a global serial number prefix that applies to all items,
click S/N Definition on
the Inventory Parameters
form.
- For a serial number prefix that applies to a specific item,
click S/N Definition on
the Items
or Multi-Site
Items form. This prefix overrides any global serial
number prefix.
- On the Prefix Definition
form, add a line for each segment of the prefix.
- To specify the segments of the prefix:
- Click in the Segment Value
field and select from the list of placeholder options. See the
table below for explanations of the options.
- You can include as many segments as you need in the prefix.
However, the serial number length is limited to 30 characters.
If you specify a prefix that could be greater than or equal
to the limit, you receive a warning.
- To include a constant, for example a hyphen, specify Constant in the Segment
Value field and then specify the character(s) in the Segment Placeholder Value field.
- To change the order of the segments, click the Up
and Down buttons.
- The full prefix (using placeholders) is displayed in the Prefix field.
- Click OK to return to the
previous form, where the prefix is displayed in the S/N
Prefix field.
Prefix Segments and Placeholders
On the Prefix
Definition form, select from the options in this table to create
the segments of the prefix. After you specify the segments and the order,
they display in the Lot Prefix
or S/N Prefix field as tokens,
or placeholders, that are replaced by the assigned values when the numbers
are actually generated. See our examples.
NOTE: We recommend
that Ref Num, Ref Line/Suffix, and Ref Release placeholders should be
followed by a constant value of a hyphen (-) to ensure that results are
as expected. We suggest that you use a hyphen because many other characters
cannot be read in a bar code.
Placeholder |
Option Description |
Number of characters |
Notes |
| &M |
Month |
2 |
|
| &D |
Day |
2 |
|
| &Y |
Year |
2 |
|
| &Z |
Year |
4 |
|
| &T |
Reference Type |
1 |
Character value based on the transaction type:
C - Project
I - Inventory(JIT/Kanban, Misc Receipts, etc.)
J - Job
O - Customer order
P - Purchase order
R - RMA
S - Production schedule
T - Transfer order |
| &N |
Reference Number |
10 (TRIM) |
Value based on the transaction type:
Project number
Inventory - None
Job number
Customer order number
Purchase order number
Production schedule number
Transfer order number |
| &L |
Reference Line or Suffix |
4 |
Value based on the transaction type:
Project task
Inventory - None
Job suffix
Customer order line number
Purchase order line number
RMA line number
Production schedule - None
Transfer order line number |
| &R |
Reference Release |
|
Value based on the transaction type:
Project sequence
Inventory - None
Job - None
Customer order line release (if 0 then none)
Purchase order line release (if 0 then none)
RMA - None
Production schedule - None
Transfer order - None |
| &S |
Site |
8 (TRIM) |
Alphanumeric site ID |
| && |
Literal Value "&" |
1 |
|
| (Constant) |
Constant value |
|
Specify a value in the Placeholder Value field. These are static
characters that are included in the prefix. For example,
you can use a hyphen (-) to separate the segments, or include
SN- to indicate that this is a serial number. |
Related Topics
Creating Lot Tracked
Inventory Items
Preassigning Lot Numbers
Tracing Lot-Controlled
Materials