NOTE: See Writing a Custom Scheduler Rule for a summary of the steps required to create custom rules. For more details about the functions described in this topic, see the Simulation Tailoring Support Function Reference (available for download from the Support web site, on the documentation page for the Infor APS Virtual Planning/Simulation product).
Job release rules determine the sequence of scheduling for jobs with the same release date and time.
Your custom function can have any name that is not a standard user-callable function name.
#include "factor.h" double myrule(op) ORDER *op; /* pointer to the job. */
This function must accept a job (Type: ORDER*) as its only argument.
The function should return the ranking value of the job (Type: double).
double orrl (ORDER *op)
/*-----------------------------------------------------------------
Ranking function to cause new jobs to be ranked on a high-to-low priority.
ARGS:
op - pointer to job for which to evaluate ranking rule
RETURNS: job-ranking value
-----------------------------------------------------------------*/
{
return((double) -op->orprio);
}
To make your custom job release function available to the Scheduler, you must "install" it from the initialization function ucini1 by calling the function sedfok. The function sedfok has two arguments:
For example, to install the above example rule "orrl" in rule position 39:
sedfok (39, orrl);
Compiling and Linking Custom Scheduler Rules