Current Operations

Use the Current Operations form to maintain routing requirements and costing information for an item. In addition, you can create and maintain the list of resources required to perform an operation (for APS planning and for the Scheduler). You can then use this information as a template for the standard method of manufacturing the item (when you define the job operations and materials). When you delete the current operation, the system deletes the operation and all associated materials and material references.

Use the Standards tab to maintain or view routing requirements for an item. Use the Resources tab to maintain the list of resource groups that can work on this operation. An operation must specify at least one resource group. Use the Costs tab to maintain cost rates of the operations.

NOTES: The Standard Operations form maintains the costing information for the routing. If you want to update the costing information for the standard operation from the current operation information, you must run the Roll Current Cost to Standard Cost utility.

If the ECN Use for Current BOM/Routings inventory parameter is set to All, you cannot add or make changes to current operations.

The fields on the Resources tab applies only to APS and the Scheduler.


Related Topics

Copying Routings/BOMs

Creating Outside Operations

Creating Routings and Bills of Material

About Operation Run Time - Planning and Scheduling

Creating Outside Operations

Creating a Setup Matrix

Defining Overlapping Operations

Operation Setup Time Overview

Splitting a Job Across Resources

Scheduler Batching