Use this event handler to automatically notify certain SyteLine users when an engineering change notice is created on the Engineering Change Notices form. The message also prompts for a Yes/No response to approve the change. Based on the response, the event handler sends an approval or rejection notification to the originator. Both notifications are messages sent to the SyteLine Inbox form.
This is the text of the notification that is sent:
To: receipient From: originator Subject: Engineering Change Notice approval request Body: Approval has been requested for Engineering Change Notice ecnnum, created by originator, with the priority of ecnpriority. Question: Do you approve the Engineering Change Notice? Choices: Yes and No.
If the response is Yes, this message is sent to the originator's SyteLine Inbox:
To: originator From: receipient Subject: Engineering Change Notice approved Body: Engineering Change Notice ecnnum has been approved.
If the response is No, this message is sent to the originator's SyteLine Inbox:
To: originator From: receipient Subject: Engineering Change Notice rejected Body: Engineering Change Notice ecnnum has been rejected.
| Variable | Description |
|---|---|
| recipient | This is the SyteLine user name you specify in the Notify Users field on the Workflow Event Handler Activation form. You can specify multiple names separated by semicolons. |
| originator | This is usually the name of the SyteLine user who performed
the action that generated the message.
However, if the system cannot determine a user associated with the action, a default address or name is used. In some cases, this default is the SMTP User Name associated with the intranet entered on the Site/Entities form for the site. |
| ecnnum | This is the number for the proposed Engineering Change Notice. |
| ecnpriority | This is the value of the Priority field on the Engineering Change Notices form. |
To change the subject or body of the messages, see Modifying Workflow Event Handlers.
This global constant is created by the event handler, based on the entries you make in the Workflow Event Handler Activation form:
| Global Constant | Contains |
|---|---|
| ECNApproverID | Contents of the Notify Users field |
The event IdoOnItemUpdate for the SLEcns IDO triggers this notification.