Use this event handler to automatically notify certain people when the due date is changed on an invoice. The notification can be an external e-mail and/or a message sent to the Inbox form for SyteLine users.
This is the text of the notification that is sent:
To: receipient From: originator Subject: AR Invoice due date change Body: The Due Date for Invoice invoicenum for Customer custnum, custname has been changed from oldduedate to newduedate.
| Variable | Description |
|---|---|
| recipient | For a SyteLine Inbox message, this is the SyteLine user
name you specify in the Notify Users field on the Workflow
Event Handler Activation form. You can specify multiple
names separated by semicolons.
For an external e-mail, this is the e-mail address you specify in the E-mail Users field on the Workflow Event Handler Activation form. You can specify multiple names separated by a semicolons. |
| originator | For a SyteLine Inbox message, this is usually the name
of the SyteLine user who performed the action that generated
the message.
For an external e-mail, this is usually the e-mail address associated with the SyteLine user who performed the action that generated the message. However, if the user does not have an associated e-mail address in the Users form, or if the system cannot determine a user associated with the action, a default address or name is used. In some cases, this default is the e-mail address for the SMTP User Name associated with the intranet entered on the Site/Entities form for the site. |
| invoicenum | This the invoice number, shown on the Invoices, Debit and Credit Memos form, where the due date changed. |
| custnum | This is the number of the customer on the invoice where the due date changed. |
| custname | This is the name of the customer on the invoice where the due date changed. |
| oldduedate | This is the value of the Due Date field on the invoice before it was changed. |
| newduedate | This is the value of the Due Date field on the invoice after it was changed. |
To change the subject or body of the message, see Modifying Workflow Event Handlers.
These global constants are created by the event handler, based on the entries you make in the Workflow Event Handler Activation form:
| Global Constant | Contains |
|---|---|
| InvoiceDueDateManagerID | Contents of the Notify Users field |
| InvoiceDueDateManagerEmail | Contents of the E-Mail Users field. |
The event IdoOnItemUpdate for the SLArinvs IDO triggers this notification.