Use this event handler to automatically notify certain people when a new customer was added on the Customers form. The notification can be an external e-mail and/or a message sent to the Inbox form for SyteLine users.
This is the text of the notification that is sent:
To: recipient From: originator Subject: New Customer Body: New Customer custnum has been created.
| Variable | Description |
|---|---|
| recipient | For a SyteLine
Inbox message, this is the SyteLine
user name you specify in the Notify Users field on
the Workflow
Event Handler Activation form. You can specify multiple
names separated by semicolons.
For an external e-mail, this is the e-mail address you specify in the E-mail Users field on the Workflow Event Handler Activation form. You can specify multiple names separated by a semicolons. |
| originator | For a SyteLine
Inbox message, this is usually the name of the SyteLine user who
performed the action that generated the message.
For an external e-mail, this is usually the e-mail address associated with the SyteLine user who performed the action that generated the message. However, if the user does not have an associated e-mail address in the Users form, or if the system cannot determine a user associated with the action, a default address or name is used. In some cases, this default is the e-mail address for the SMTP User Name associated with the intranet entered on the Site/Entities form for the site. |
| custnum | This is the new customer number that was added on the Customers form. |
To change the subject or body of the message, see Modifying Workflow Event Handlers.
These global constants are created by the event handler, based on the entries you make in the Workflow Event Handler Activation form:
| Global Constant | Contains |
|---|---|
| NewCustomerCreatedManagerID | Contents of the Notify Users field |
| NewCustomerCreatedManagerEmail | Contents of the E-Mail Users field. |
The event IdoPostItemInsert for the SLCustomers IDO triggers this notification.