In general, customer amounts will be stored in the system in the customer's currency. This affects CO, Estimating, and Accounts Receivable.
Vendor amounts will be stored in the vendor's currency. This affects purchase orders and accounts payable.
Cash accounts in Bank Reconciliation may be stated in non-domestic currencies. When receiving customer payments or making vendor payments, you may specify the payment with either domestic currency or the customer/vendor currency.
All amounts in journals, ledger, inventory (price and cost), and the shop floor are always stated in domestic currency.
NOTE: When amounts are posted into journals they are translated.
Generating Voucher (PO) and Posting Vouchers (A/P) - When the voucher record is created, the system stores any change in exchange rate from receiving time to voucher generation time as a distribution. The voucher is stored in the vendor's currency. When the voucher is posted, domestic amounts are posted to the journal and vendor amounts are put on the posted transactions record along with the exchange rate that was used for posting.
Payment - Payments may be entered in either the Domestic Amount or Vendor's amount based upon the currency code of the Bank Code you select for the payment. When the payment is posted, domestic amounts get posted to the journal, and vendor amounts are put on the Posted Transaction record. At payment posting time, a mini-gain/loss is performed for the voucher and any payments or adjustments to that voucher. All of the posted transactions tied to the voucher will be "upgraded" to the new exchange rate.
The voucher's Gain/Loss is posted to either Loss (Debit) or Gain (Credit)
Invoice Printing (CO) and Posting (A/R) - When the invoice record is created, any change in exchange rate from Shipping time to invoice printing time is stored as a distribution. The invoice is stored in the customer's currency. When the invoice is posted, domestic amounts are posted to the journal and customer amounts are put on the Posted Transaction record along with the exchange rate that was used for posting.
Payment - Payments may be entered in either the domestic amount or the customer's amount based upon the currency code of the Bank Code you select for the payment. When the payment is posted, domestic amounts get posted to the journal, and customer amounts are put on the Posted Transaction record. At payment time, a mini-gain/loss is performed for the invoice and any payments, debits or credits to that invoice. All of the Posted transactions tied to the invoice will be upgraded to the new exchange rate.
Difference to currency Loss (Debit) or Gain Account (Credit)
At various times, you may wish to recognize any outstanding Gains or Losses. Run the Gain/Loss utility and specify either A/R, A/P or both.
A/R - Process all Posted A/R Transactions and upgrade them to the current exchange rate. For each invoice that has a gain or loss, post the amount to Accounts Receivable and the Gain or Loss Account.
A/P - Process all outstanding PO Receipts (received but not yet vouchered) and upgrade them to the current exchange rate. For each record that contains a gain or loss, post the amount to Vouchers payable and the Gain or Loss Account.
Process all unposted vouchers and upgrade them to the current exchange rate. For each voucher that has a gain or loss, post the amount to Vouchers Payable and the Gain or Loss Account.
For Gain/Loss Accounts:
The system contains a currency master file where all currencies are maintained. Users may enter an unlimited number of date- and time-stamped currency exchange rates. They may also back-date these rates by entering a past date. There are two exchange rates entered. The Buying rate is used exclusively in PO and A/P. The selling rate is used exclusively in CO, Estimating, and A/R.
Users are able to print Financial Statements in different currencies. The exchange rates used to print the report are the rates stored in the database that contains the ledger records being processed. The translations are for display purposes only. No posting of any kind takes place and no gain or loss is calculated.
Translations are defined for each line of the financial statement. Users choose to use the Buying or Selling Exchange rate. They choose one of the following translation methods: