Multi-Currency Setup
If you will be dealing with customers or vendors who
use currencies other than your base (domestic) currency, use the following
process to set up exchange rates and other multi-currency features.
- Make sure the general ledger accounts specific to currency exchange
are set up in the Chart
of Accounts:
- Realized Gain
- Realized Loss
- Unrealized Gain
- Unrealized Loss
- A/R Unrealized Offset
- A/P Unrealized Offset
- V/P Unrealized Offset
If you are not using Unit Code 4 for anything else, you might want
to set Unit Code 4 to Accessible for these accounts, and use it for
reporting the foreign currency impact of the different currencies.
If you do this, the currency codes must be entered for Unit Code 4.
For information about setting up unit codes, see Account
Unit Code (1-4).
- Set up currency and exchange rate variance accounts for the domestic
currency and the Euro on the Multi-Currency
Parameters form, to help you track realized and unrealized gains
and losses due to exchange rate changes. These accounts should match
the ones you set up in step 1. During installation, you set up a Site
Currency Code, which is the domestic currency code shown on this form.
- Set up all other required currencies used by your vendors and customers
in the Currency
Codes form.
For each currency code, the unrealized and realized G/L accounts
specified on this form default to the accounts set up in the Multi-Currency
Parameters form. You can also designate expenses by currency code
if you use unit code 3 or 4.
- Use the Currency
Rates form to enter exchange rates between all currencies you
set up in step 3 and the To currency. On the Currency Rates form,
the To Currency field is typically your domestic currency.
- Use the Bank
Reconciliations form to set up bank codes and accounts to use
with foreign currency customers and vendors. The bank reconciliation,
attached to the bank code, maintains a record of all receipts and
payments for each currency/bank code. If you will be recording A/R
or A/P payments in foreign currencies, you should set up the foreign
bank codes (with applicable currency codes) on the Bank Reconciliations
form. Then you can include those foreign bank codes on customer and
vendor records.
- Use the Customers
and Vendors
forms to set up foreign currency customers and vendors.
- If your system will share currency information between multiple
sites, set up Replication
Rules for the Shared Currency replication category.
After Setup
- Enter foreign currency customer orders and purchase orders. To
see the amounts translated to your domestic currency, use the associated
Domestic
Currency forms.
- Periodically, update the exchange rates and run the Currency
Revaluation Utility. This utility uses the current exchange rate
(from the Currency Rates form) to determine gains and losses due to
currency fluctuations.
Related Topics
Multi-Currency
Overview
Converting
the Domestic Currency to the euro
Customer
Orders and Invoices in Foreign Currencies
Setting
Up the Euro Currency Code
About
Currency Conversions for Transfer Orders
About
Realized and Unrealized Gains and Losses
Currency
Revaluation Utility
Domestic Currency
Euro Currency
Overview
How
the System Handles Multi-Currency Transactions