To perform simple, quick movements of inventory where there is relief of inventory in one site and receipt in another, use the Multi-Site Quantity Move form. A multi-site quantity move does not require paperwork and assumes no transit time. It is frequently used in Focused Factories or close proximity locations. All material and financial transactions occur automatically without user intervention. These moves may be:
If these conditions are not met, the system uses the Unit Cost.
Multi-Site Quantity Moves can be either Push or Pull transactions.
Push transactions move material from Site A to Site B.
EXAMPLE: Site A is the originating site and moves material to Site B. Site A is considered the From Site and Site B is considered the To Site. The transaction uses the cost/price of Site A.
Pull transactions move material from Site B to Site A.
EXAMPLE: Site A is the originating site and moves material from Site B. Site A is considered the To Site and Site B is considered the From Site. The transaction uses the cost/price of Site B.
The system provides functionality for any one site to enter a Multi-Site Quantity Move for items to be moved at that site from one other shipping site.
NOTE: The following convention is suggested when you are performing a Multi-Site Quantity Move.
The Multi-Site Quantity Move form prompts for both From and To Locations. However, frequently you might not know a valid To Location. Therefore, we suggest that you use the location staging in one or both locations.
For example, if you are at Site A and performing a Multi-Site Quantity Move to Site B, when the form prompts for a receiving location, enter Staging. If the Staging location is consistently used, then the user at Site B will always check the Staging location for incoming items or materials as a result of Multi-Site Quantity Moves.
Costing functionality begins by performing validations for proper account numbers set up at both the From and To Sites. The transaction date is checked against the dates for the current accounting period.
When items or materials are moved between two different entities, the transaction can use either the Unit Cost or a price. For many moves the Unit Cost is sufficient, and in that case you are not required to enter the Unit Cost. However, you must enter two Price Codes if you wish to indicate a price:
The Multi-Site Quantity Move checks these two Price Codes, and if a match is found then the Price Matrix is searched and the appropriate Price Formula is used for costing.
Material Transactions records and journal entries are also created. For Multi-Site Quantity Moves there is no timing issue involved for posting journal entries because there is no transit time. Therefore, when a Multi-Site Quantity Move is entered, journal entries are created for both the To and From sites and they are both posted at the same time.
The following table outlines what types of moves and types of costing and pricing Multi-Site Quantity Move supports.
| Cost Type | From Loc to Loc | From Whse to Whse | From Site to Site | From Ent to Ent |
|---|---|---|---|---|
| 1 - Same Cost | yes | yes | yes | yes |
| 2 - Different Cost | * | * | yes | yes |
| 3 - Price or Cost | no | no | no | yes |
Key:
* = Specific Costing only
Loc = Location
Whse = Warehouse
Ent = Entity
In determining which Unit Price to use on a Multi-Site Quantity Move, several validations take place by the system. The following conditions are assumed:
The system checks for matching Price Codes as defined on the Item Pricing form and for the From Site and To Site combination as defined on the Inter-Site Parameters form.
NOTE: The system checks the Item Pricing form for the item at the From Site.
When a match is made for the Price Codes, then the system searches the Price Matrix for a valid Price Formula and uses it for price calculations. If no valid Price Formula is found, then the Unit Cost is used.
Journal entries are made automatically based on the accounts defined in the Inter Site Receive To Accounts and Inter Site Ship From Accounts.
In order to perform a Multi-Site Quantity Move, it is necessary for both the From Site and To Site databases to be running and connected to the global database. If these conditions are not met, then error messages display and indicate that this option is not currently available. You are prevented from performing this transaction until the condition is corrected.
If an error condition occurs during a Multi-Site Quantity Move, (for example, one of the databases becomes disconnected), an error message displays and the transaction is not completed. The entire transaction is backed out and you must repeat it later when the necessary conditions have been re-established.
NOTE: If previous transactions have been successfully completed, they are not backed out when an error condition occurs. The only transactions that fail will be the ones that were being entered at the time of the error condition.
You can correct or reverse a Multi-Site Quantity Move by entering a Quantity Adjustment at each site. This corrects the inventory, but not the accounting. The accounting must be manually corrected based on your situation and the type of costing that you use.
Multi-Site Quantity Moves create accounting transactions automatically without user intervention. The following chart summarizes the accounts that are affected based on the type of move (for example, entity-to-entity moves, site-to-site moves, etc.). The cost used is also a variable. For example, the cost can be the same between two sites. When reading the chart, refer to the following key:
Key:
All = These accounts will record transactions for all costing conditions. In the case where the cost is the same for both the From and To Sites, then these are the only accounts that will have transactions.
y = The 'y' indicates that for this type of transaction this account will be affected.
* = Variances are recorded in the Val Var account when using Standard Costing.
NOTE: Variances are recorded in the Inv Adj account when using Actual costing.
Cost Variables:
cost<>cost = From Site and To Site have different costs
price <>cost = From Site charges the To Site a price
| Sales | COS | A/R | Profit | Cost | A/R | A/P | Split-WIP | ValVar | InvAdj | CIring | |
|---|---|---|---|---|---|---|---|---|---|---|---|
| Ent to Ent - All | Y | Y | Y | Y | |||||||
| Ent to Ent - cost <>cost | Y | Y | |||||||||
| Ent to Ent - price <> cost | Y | Y | |||||||||
| Site to Site - All | Y | Y | |||||||||
| Site to Site cost <> cost | Y | ||||||||||
| Whse to Whse - All | Y | ||||||||||
| Whse to Whse - cost <> cost | Y |
Lot tracking is independent for each site. This means that each site creates/maintains lot numbers for that site only. There is not a common pool of lot numbers that is shared across all sites.
In order to perform lot tracking, you need:
NOTE: This permits you to create item locations and item lots 'on the fly' for the To Site.
When doing either site-to-site or entity-to-entity moves, enter the lot number when you specify the To Lot. The system carries forward the lot number from the From Site to the To Site. Matltrack records are created automatically by the system, which can then be used to trace these transactions at a later time.
Serial Number Tracking assumes that serial numbers are corporate-wide and are not independent for each site. This means that each site creates/maintains serial numbers that are used by all sites.
To perform Serial Number Tracking, you need:
NOTE: This permits you to create item locations 'on the fly' for the To Site.
When doing either site-to-site or entity-to-entity moves, enter the serial number when you specify the To Location. The Serial Number tab is enabled. Matltrack records are created automatically by the system which can be used to trace these transactions at a later time.
The following table presents your options for entering serial numbers.
| From Site | To Site Yes-Serial Track Enabled |
To Site No-Serial Track Not Enabled |
|---|---|---|
| Yes-Serial Track Enabled | From Site-user selects s/n and processes To Site- process SAME s/n |
From Site-user selects s/n and processes To Site- Not Valid Option |
| No-Serial Track Not Enabled | To Site-user enters NEW s/n and processes | Not Valid Option |
NOTE: When the To Site has serial numbers enabled but the From Site does not, enter new serial numbers in the Serial Numbers tab after the To Loc and To Lot fields are entered.
The following Matltran records are created for each type of move as indicated in the following table:
| Move | Type | Ref |
|---|---|---|
| loc/loc | M | I |
| whse/whse | M | I |
| site/site | M | I |
| entity/entity | M | I |