Projects

Use the Projects form to enter a project header.

WIP Relief Tab

WIP project costs are relieved when the Revenue Recognition Milestones or the WIP Relief Post Utility is run.

WBS Tab

This tab contains a read-only grid showing the Work Breakdown Structure and the WBS description

Tax Info Tab

If your system is set up for only either item or area based tax mode, only one tax code field displays in this tab.

Some of the fields on this tab are used by the European Union (EU). If the Activate EU Reporting field on the General Parameters form is not selected, some of these fields are disabled.

Percent Complete and Percent Complete Details Tabs

The information on the Details tab differs from the Percent Complete tab in that it is broken down by cost code AND monthly period, giving you even more detail than is on the Percent Complete tab.

Actions Menu

The Actions menu includes options to filter the data to show only projects where the start date is 7, 14 or 30 days in the future, and an option to show only projects where the start date is any number of days in the past.


Related Topics

Projects Overview

Create A Project