Tax Interface Parameters

Use this form to set up information and default values for tax interfaces and to turn debugging on and off for the interface.

Depending on which tax system you select on the General tab, certain Parameter tabs are enabled so you can enter more setup information for use with that tax system.  The Debugging tabs are also enabled or disabled depending on the tax system selection.

The Warehouse tab allows you to specify the county where a warehouse is located, for more accurate taxation.


Related Topics

About the Tax Interface

Setting up a Vertex Tax Interface

Setting up an AvaTax Tax Interface

Setting up a Taxware Tax Interface

Setting up a Taxware Enterprise Tax Interface

Debugging Tax Calculations

Setting Up Default Tax Codes