About the Tax Interface
If you require external taxing software to handle the computing of sales
tax, you can use the Tax Interface, which supports these products:
- Vertex Sales Tax Q Series
- Taxware Sales/Use Tax System
- Taxware Enterprise
- Avalara AvaTax
In SyteLine,
the tax interface is a separately licensed and installed product. To access
the tax interface forms, you must be a licensed SyteLineTax user.
The Tax Interface is configured for the appropriate product with the
Tax
Interface Parameters form. After the interface is configured,
taxes are automatically calculated on customer
orders where the tax code is set to EXTRNL.
(The EXTRNL tax code is added automatically to the Tax Codes
form at a site when you enable the SyteLineTax module on the Optional Modules
form.)
After the orders are invoiced, and before posting is performed, you
must run the Tax
Interface Post Register utility to post the taxes to
the external tax software.
If taxes are not being calculated correctly, you can use the Debug fields
on the Tax Interface Parameters
form to create log files that can help either Infor support or the appropriate
tax system support to assist you.
If you are using AvaTax,
use the Tax
Interface Invoice Tax Credit form to give tax-exempt customers
credit for taxes after an invoice has been created with taxes calculated.
What Information does the Interface Send to the Taxing Software?
Any order, RMA, invoice, credit memo or other information where the
first tax code is set to EXTRNL is sent to the interface. (For compatibility
with older versions of this interface, a tax code of VERTEX also causes
taxes to be processed by the interface.) On the Tax
Interface Parameters form, click Set All Customer Tax Code 1
to External to perform a system wide change that substitutes the selected
tax interface in place of everything currently set to Tax Code 1.
The Tax System Interface can send this information, based on your selections
on the Tax Interface Parameters
form:
- Customer information: The interface sends this information from
the Customer Ship To record: Customer Number, City, State, Zip, County
- Warehouse Information: If the warehouse can be determined, the
City, State, Zip, and County of the warehouse is sent, as well as
the Warehouse Code. This allows for more accurate taxation. If
the warehouse is not available, the address information from the General
Parameters form is sent. You
can also use the Warehouses tab on the Tax Interface Parameters
form to specify the county where a warehouse is located.
- Item Information: Either Item or Product Code is sent based on
the setting of the Send for Product
field in the Tax Interface Parameters
form.
- Freight and Miscellaneous Charges for Items: Freight is passed
into your external tax system with the Freight flag set and the Item
Number set to FREIGHT. Miscellaneous charges are sent with the Item
Number set to MISC CHARGE
- Miscellaneous and Labor Charges for Service: Miscellaneous and
Labor Service transactions use the Exclude
Field Service Misc and Exclude Field Service Labor options
on the Tax Interface Parameters
form. If an option is selected (set to Exclude), then for all tax
providers except the Taxware Sales/Use Tax System, the system sends
SVC-MSC-EXEMPT or SVC-LBR-EXEMPT. For the Taxware Sales/Use Tax System,
the system sends 89999 for both Labor and Miscellaneous Charges. If
the options are not selected, indicating that the charges should be
included, then the system sends the Misc/Work codes from the transactions.
Related Topics
Setting Up a Tax
Interface
Debugging Tax Calculations
Crediting Tax-Exempt
Customers
Setting
Up Default Tax Codes