A Project transaction allows the employee to enter a Labor transaction for a Project defined on the Projects form.
There are other ways of charging labor to a Project other than through a Project transaction. It can be done through Run, Setup, Direct, and Multi-Job transactions. These types of transactions can be used if the job that is charged the Labor transaction is cross referenced to a Project Task.
A Project transaction is necessary when labor is to be charged directly to the Project and Task, without the need for a job. Examples of this are to charge Engineering time or Project Management time to a Project Task. During the Project transaction, the employee punches into the Project Number and the Task Number.
For more information on Projects and Project Costing, please refer to the Project Management topic in the Infor SyteLine Online Help.