Shop-Trak Defining Background Parameters
Use the Background tab of the
Shop-Trak Parameters
form to define options on how Shop-Trak Background Polling automatically
transfers and posts transactions to Infor SyteLine.
To define Background parameters:
- Open the Shop-Trak Parameters
form.
- Click the Background tab.
- Specify this information:
Polling
Controls
- Polling Enabled
- Select this check box to enable Background Polling. Enabling
this field creates an SQL job on
the SQL server. The SQL Server Agent must be running to start the
polling.
- Daily Start Time
- Specify (in Military format) the time you want Background
Polling to begin. Polling will start as soon as the
SQL server reaches the start time.
- Daily End Time
- Specify (in Military format) the time you want Background
Polling to stop.
- Frequency - Specify
how often in minutes you would like Background Polling to
run (use whole integers only). The Frequency can be
set and maintained to accommodate the transition of organizations
from batch related systems to real-time.
- Last Polling -
This field is read-only and displays the last date and time
Background Polling ran.
- Transfer to SyteLine Unposted
- This check box will be selected by default upon installation
of Shop-Trak. It allows Background Polling to automatically
do the following when the Transaction Type is enabled in the
Transfer/Post Options box:
- Transfer Run, Indirect, Setup, Move, and Direct transactions
from the Shop-Trak Edit Transactions form to the
Unposted Job Transactions
form.
- Transfer Project transactions to the
Project Labor Transactions form.
- Post Work Center Transactions to Infor SyteLine.
- Transfer Service Repair Orders to the SRO
Transactions form.
- Transfer to SyteLine Locked
- If a circumstance arises that locks the Background Polling,
this field will become checked. To unlock Background
Polling, click Unlock.
You can use the Background
Polling Log to monitor Background Polling activity.
If polling becomes locked, a message displays in the
log.
Posting
Controls
- Post Unposted Transactions
- This field determines which transactions to post from
the Unposted Job Transactions
and Project Labor Transactions
forms.
- N (None) -
Select N to have no transactions post. Transactions
will accumulate until manually posted.
- A (All) -
Select A to have all transactions post (both transactions
transferred automatically from Shop-Trak and those entered
on the Unposted Job Transactions
form).
- O (Only)
- Select O to post only those transactions that
transferred automatically from Shop-Trak using Background
Polling.
- Issue to Parent
- This field determines when to issue completed quantities
from the sub-job to the parent job.
- A
(Always) - Select A to always issue completed
quantities to the parent job when the sub-job completes.
- N
(Never) - Select N to never issue completed quantities
to the parent job; sub-job quantities will go to
inventory instead.
- B (According to BOM) - Select B to issue quantities
according to the parent's Bill of Materials (BOM). The
parent is checked to see if it is set to backflush. If the parent is set to
backflush, the completed
quantities on the sub-job will
not issue to the parent. If the parent is
not set to backflush,
the completed quantities on the sub-job will
issue to the parent.
- Post Project Transactions
- Select this check box to automatically post Project transactions
or leave the box cleared to post Project transactions manually.
If Project transactions post automatically, the Project Transactions Report
will not print.
- Post Complete Trx's - Select this check box to indicate
if Complete transactions should be posted to Infor SyteLine.
A Complete transaction is one in which the transaction's
Operation Complete and/or Job Closed have been set to Yes.
When you select the Post Complete Trx's
check box, both completed and non-completed transactions will
post. If this check box is not selected, only transactions
that do not complete the job or operation will post.
- Post Negative Inventory
- Select this check box to allow the Material quantity on
hand to become negative after
the posting of a transaction. If this check box
is not selected, a transaction that will result in negative
on-hand quantities will not post.
Transfer/Post Options
- Transaction Types
- Run, Setup,
Indirect, WIP
Move, Service Repair
Order, Project, Team, Work Center, and Direct. Select the
check boxes of the Transaction Types you want to transfer
and post to Infor SyteLine. Any combination is
valid.
- Employee Types
- Hourly, Non-Employee,
or Salaried. Select
the check boxes of the Employee Types you want to transfer
and post to Infor SyteLine.
- Ranges - Specify
the Starting and Ending Job,
Date, Employee,
Dept,
and Shift of the transactions
you want to transfer and post to Infor SyteLine. This
is useful when first installing Shop-Trak to verify procedural
accuracy before establishing them company-wide. Leaving
the fields blank will transfer and post all transactions not
previously filtered out.
Background Task Submission
This
section contains settings for inventory and material transactions
(JIT, Job Material, Prod Sched Complete, and Work Center Material) processed
by Infor Framework TaskMan.
- User ID - Select
the SyteLine User ID that you want to associate with these transaction
types. If no user is specified, this field defaults
to SA.
Post
Pending Inventory & Material Transactions
These
check boxes will be selected by default to post pending inventory and
material transactions automatically:
- Job Material Transaction
- Just in Time Production Transaction
- Work
Center Material Transaction
- Production Schedule Transaction
To prevent automatic posting, clear any or
all of the check boxes. Clearing the check box will hold the transactions
in the associated Shop-Trak pending inventory or material transactions
form until they are manually resubmitted.
IMPORTANT:
It is recommended that you have employees log out of Shop-Trak
before changing this parameter. Otherwise, transactions might not
post as expected.
- Save your changes and
close the form.
Related Topics
Shop-Trak Parameters Form
Viewing the Shop-Trak
Background Polling Log
Shop-Trak Transaction Flow
Chart
Shop-Trak Transaction
Flow Overview
Shop-Trak Reviewing Pending
Inventory & Material Transactions