Shop-Trak SyteLine Supporting Forms

This topic lists and describes the SyteLine forms and concepts that are used with Shop-Trak.

Shift Codes Form

Zero Shift Master Definition

Unposted Job Transactions Form

Employees Form

Other SyteLine Master Files

Shift Codes Form

Defines individual shifts (1st shift, 2nd shift, etc.).  The shift code referenced for Shop-Trak transactions is the shift defined within the employee's master file.   These shifts are utilized within Shop-Trak to determine Shift Premiums, Holiday Factors, Applying Premiums to Manufacturing Rates, Shift Start and Stop Times, Pay Basis, and Grace Periods of each employee's transaction.  An unlimited number of shifts can be added for flexibility in adapting unique work schedules. information about those transactions that still reside in the Shop-Trak Edit Transactions form.  There are multiple range options available when generating this report including employee, transaction type, dates, job, shift, department, and indirect code.  

Shift Code Form Fields

 

Shift

NOTE:  See Zero Shift Master for non-defined (flexible) shifts.

Lunch

Grace periods for employees can be defined for rounding in and out times of labor transactions.

 

Additional Shift Code References

The Shop-Trak Time Attendance / Delinquency Report utilizes the Shift Code Start and End times to determine exceptions of employee transactions (Early In, Late Out, etc.).

 

NOTE:  Lunch times are determined from the Shop-Trak Break Lunch Schedule form and not from the SyteLine Shift Codes.

Zero Shift Master Definition

A Zero Shift Master is a shift master with Hours, Start, and End times defined as zero.  This is applicable to an entire week or specified days of the week.  

Shop-Trak utilizes a Zero Shift Master as a flexible shift designed for organizations that have employees working with flexible start and end times.  When punching in for the day, times always round forward in the increments defined by the Early In/Late Out field.  Punching out for the day always rounds times backward in the increments defined by the Early In/Late Out field.  The Late In/Early Out field is completely ignored when using the Zero Shift Master.  Administrators may set up as many zero shifts necessary to utilize different rounding increments and name them as they wish.

IMPORTANT:  Set the Early In/Late Out value to a divisor of 60 minutes.  With Zero Shift Masters, no Shop-Trak Time Attendance / Delinquency Report exception messages can be utilized (i.e.: Punched in Early, Punched in Late, Punched out Early, etc.) because no start or end times are defined.

Unposted Job Transactions Form

See Shop-Trak Transaction Flow Overview.

Employees Form

General Tab

Shop-Trak validates Employee Number and Shift fields from the Employees form.  

NOTE: Temporary personnel can be added to General tab on the  Employees form (type = Non-employee) for the purposes of collecting their labor and providing time and attendance reports to the agency.

If payroll is being generated from transactions collected from the shop floor via Shop-Trak, the Generate Payroll From field must be set to Mfg Lbr.

Rates and Taxes Tab

The Mfg Reg Rate, Mfg OT Rate, and Mfg DT Rate values; along with the Shop-Trak Rate Rules, are used by Shop-Trak for labor costing.  Shop-Trak uses the Reg Rate, OT Rate, and DT Rate for Payroll processing.

Other SyteLine Master Forms

The following Infor SyteLine forms also contain information that must be set up for Shop-Trak. If you have been reporting Labor manually, this information would have already been set up.  Underneath each form is the location in the Master Explorer Modules folder.

Department Masters - Departments referenced by work center and employee records.

Employee > HR > Organization > Departments

Indirect Labor Codes – Defines the codes used when entering job transactions.

Production > Jobs > Files > Indirect Labor Codes

Scrap Reason Codes - Define codes to track the entry of manufacturing scrap.

Production > Jobs > Files > Scrap Reason Codes

Work Centers – Defines the work centers used in job routing.

Production > Work Centers > Work Centers

Jobs/Operations – Are needed to allow the employee to perform job transactions from the shop floor.

Production > Jobs > Job Orders

Production > Jobs > Job Operations

 


Related Topics

Shop-Trak Rate Change & Multi-Job Rules