Shop-Trak Transaction Flow Overview
After being entered into Shop-Trak Shop Floor, transactions flow through
different paths depending on the transaction type. Transactions
can be transferred automatically
or manually.
Transaction Flow by Type
- Indirect,
Setup, Run, Move, Direct, Project, Service Repair Order, and Work
Center - These transactions are held in the
Shop-Trak Edit Transactions
form. They are then transferred to Infor SyteLine forms or posted
to Infor SyteLine depending on the transaction type:
- Indirect, Setup, Run, Move,
and Direct - These transactions transfer to the Unposted
Job Transactions form. To view transactions
that did not transfer successfully, run the Shop-Trak
Transfer to SyteLine Report. After the
transactions transfer successfully, they are then posted to Infor
SyteLine. The User
Initials field on the Unposted Job Transactions form will indicate
that the transaction originated from a Shop Floor user by displaying
one of the following:
- LTI
for an Indirect transaction
- LTS
for a Setup transaction
- LTR
for a Run transaction
- LTM
for a Move transaction
- LTD for a Direct
transaction
NOTE:
If the transaction requires approval, the approver's
initials will display in the User Initials
field after the transaction is approved.
- Project - These
transactions transfer to the Project
Labor Transactions form. To view transactions that
did not transfer automatically using Background Polling, view
the Shop-Trak
Background Polling Log. After the transactions transfer
successfully, they are posted to the Infor SyteLine Project Module.
- Service Repair Order
- These transactions post to the Labor
tab of the SRO Transactions
form of the Infor SyteLine Service module.
- Work Center Labor
- These transactions post to the corresponding Work Center in Infor SyteLine.
NOTE:
Transactions that do not successfully transfer will remain in the
Shop-Trak Edit
Transactions form until the error condition is resolved. You
can run the Shop-Trak Transfer to SyteLine
Report to view these transactions.
- QCS Test Results - These transactions post
to the corresponding Disposition
form in the Infor SyteLine Quality module.
- Prod
Schedule Complete, JIT,
Work Center
Material, and Job
Material transactions
- These transaction types post directly to Infor SyteLine using the
Infor Framework TaskMan service. To
view transactions that did not transfer due to errors,
view the Shop-Trak Pending Prod Sched
Transactions, Pending JIT
Transactions, Pending Work
Center Transactions, and Pending
Material Transactions forms.
For a graphical representation of the transaction flow, see the Transaction
Flow Chart.
Transaction Error Conditions
A transaction will not transfer if any of the following are true:
- The transaction type is Punchin
or Multi-Job.
- The transaction has no end time or hours assigned.
- A Team transaction in which quantities have not been allocated.
- A Team transaction that has open transactions for other team
members for the same Job/Suffix/Operation.
- A Team, Run, Setup, or Direct transaction without a job and
operation assigned.
- Approval is required.
- The employee is locked.
- The employee forgot to punch out.
- The employee has an open transaction with the same Job/Suffix/Operation
for the same work date.
- The employee has a break or lunch transaction with no end time
or hours assigned.
- The transaction is missing an SRO Indirect Labor Code.
- The transaction has an invalid Cost Code.
- The transaction is not in the selected range of Transfer Options
on the Shop-Trak Parameters form's Background tab.
- Payroll Rate or Job Cost Rate is blank.
Related Topics
Shop-Trak Transaction Flow Chart
Shop-Trak Transferring & Posting
Transactions Manually
Shop-Trak Transferring &Posting
Transactions Automatically
Shop-Trak Reviewing Pending Inventory
& Material Transactions
Shop-Trak Running
the Shop-Trak Transfer to SyteLine Report
Shop-Trak Editing Transactions