Shop-Trak Workstation Profile
Use the Shop-Trak Workstation Profile
form to specify the following items for an individual workstation:
- Workstation Logon - Set
a secure logon requirement for an individual workstation. This
security feature is enabled or disabled based on the
Require Secure Logon parameter on the Main
tab of the Shop-Trak Parameters
form.
- Time Zone Source - Specify
a time zone for a specific workstation. This is a required field.
This feature is useful for companies that have workstations
in one Infor SyteLine site, but the workstations themselves are spread
out across different time zones. When
a user starts the Shop-Trak application on a workstation, the time
zone validation will occur. The
Windows logon is the Workstation logon. There
are three options for the Time
Zone Source field:
- Site - The workstation will
use the time zone defined on the Sites
& Entities form in the SyteLine database Shop-Trak
is connecting to.
- Client -
The workstation will use the time zone from the Date/Time
settings of the workstation.
- Manual -
The Time Zone field
will become available and allow Administrators to choose the time
zone specifically for that workstation.
- Run Shop Floor Maximized
- Controls how the Shop-Trak Shop Floor session is displayed at the
workstation. Checking
this option will start the application in a “Full Screen Mode.”
Related Topics
Shop-Trak Defining
Main Parameters